cancel
Showing results for 
Search instead for 
Did you mean: 

ADC External Voltage Reference - ST6232

mat
Associate II
Posted on August 07, 2009 at 12:08

ADC External Voltage Reference - ST6232

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
mat
Associate II
Posted on May 11, 2004 at 09:58

The ST6232 datasheet refers to a separate ''power supply'' for the ADC to be appplied on pins AVdd and AVss. Is this actually the PSU or the ADC reference voltage (as I think it is). Is the Power supply for the ADC actually derrived from Vdd and Vss of the MCU.

I'm planning to power the MCU from 5Vdc with a 2.5V precision reference to AVdd and AVss ............ will this work

simonharrison9
Associate II
Posted on June 10, 2004 at 09:12

Hi,

The pin is for ADC power supply decoupling only.

It is internally connected to the supply rail.

This is detailled in the datasheet

DO NOT connect a different supply, as you can imagine, bad things will happen!!

hope this helps

Simon
mat
Associate II
Posted on June 11, 2004 at 07:14

The Data sheet says this:

''AV DD and AV SS . Power is supplied to the MCUA/D converter independently from the rest of the chip using these two pins.''

I'm really confused ??
gfrancia9
Associate II
Posted on August 07, 2009 at 12:08

I am looking for ST62E32BF1 or ST62T32BB6

could help me?

you have some piece?

where can I buy them?