Other: software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I think there is a bug in the STM32CubeIDE Version: 1.4.0 Build: 7511_20200720_0928 (UTC), section “device configuration tool�?, section STMicroelectronics.X-CUBE-TOUCHGFX.4.15.0 Mode and configuration.

When Graphics Application is checked, a folders tree starting from TouchGFX, with files like GFX2.touchgfx, etc, is generated. It’s OK.When the .ioc file becomes complicated (as the example I attach), it seems that TouchGFX is replaced by Src and all...

AGendrau by Associate
  • 244 Views
  • 1 replies
  • 0 kudos

Use specific NMEA data set

Hello I have another question     I am currently working on a microcontroller project I am building a GPS tachometer which transfers the NMEA data of the GNSS 4 Click Module from Mikroe via UART to my STM32L052K6T6 and outputs it to a display   How c...

MSchmutz by Associate II
  • 413 Views
  • 2 replies
  • 0 kudos

L6566B Based Flyback Design

Hi,This is the first time I am asking on this forum.Could you please help me with Some design help.I have designed circuit with eDESIGNSUITE for following requirements.1.Input voltage:180-265VAC2.Output Voltage-17V 4.2Afrom the design, it resulted ou...

deep ch by Associate II
  • 261 Views
  • 1 replies
  • 0 kudos

DNP3 implemetation

Hi everyoneI need a library for ARM to implement DNP3 protocol. does anyone here know how should I do it? does send/receiving DNP3 packets make it possible?

Ala by Senior
  • 407 Views
  • 0 replies
  • 0 kudos

How do I use the STM32CubeIDE and TrueAtollic Studio?

Hello everyone, I really need help in using STM32Cube IDE and TrueAtollic Studio. I have searched up and down on YouTube, and I haven't found a single good video on how to use these IDE's. So I am using a STM32F030R8T6 and ST-Link V2 programmer-(http...

Sashvat by Associate II
  • 297 Views
  • 2 replies
  • 0 kudos

L6983N50QTR adjusting inductor and output caps

Hi,Ive been trying to use eDesignSuite to verify my design with L6983N50QTR. Please find my schematic attached. My specs are:ICL6983N50QTRTopologybuckInput7 - 33 VOutput 15 V (2 % ripple) - 1.9 A maxWhen I put the values that I am trying to use, I ge...

NNara.1 by Associate
  • 506 Views
  • 3 replies
  • 0 kudos