Resolved! What is 3.3V Vref in this circuit design of A6986? Do I need to supply 3.3V to this pin?
https://eds.st.com/dcdc/I want 9-30V to 8V and I don't have any 3.3V voltage in my circuit. Is it okay if I don't connect anything here?
https://eds.st.com/dcdc/I want 9-30V to 8V and I don't have any 3.3V voltage in my circuit. Is it okay if I don't connect anything here?
Without eDesignSuite, our company cannot make final adjustments. Not successful trial production in June this year?
We are currently using the Ublox M8 receiver and are in the process of qualifying the Teseo-LIV3 as a possible replacement. One issue I'm having is the need to up the baud rate after initially connecting and configuring the receiver. The Ublox M8 d...
The only place I see future leap seconds mentioned, in the software manual, is in the GLONASS almanac message:KP Notification on forthcoming leap second correction of UTCAs I mentioned above, I would rather not have to request and then parse this alm...
STM-Studio is a great tool however not being able to print arrays is very frustrating. It would be very important to have this feature. Thanks in advance.
Dear All, I have one question. I can not change Number of strings using LED2000 in eDesignSuite.LED2000 can not connect LED by parallel. Can it only connect LED by serial?I always thank you for your support.
Hello,we bought an STEVAL-IPFC01V1 board as reference design for a new product. Now we would like to tune some parameters in the STNRGPFC01 firmware but the IC seems to have disappeared from eDesignSuite. Even a project created with eDesignStudio som...
can anyone suggest that which is the best for battery application linear regulator or switching regulator.Regulator specifications should be 1) Input voltage 5V-48V 2) 2A current rating3) Output voltage 5V.3) Ultra low Quscient current.please suggest...