cancel
Showing results for 
Search instead for 
Did you mean: 

I think there is a bug in the STM32CubeIDE Version: 1.4.0 Build: 7511_20200720_0928 (UTC), section “device configuration tool�?, section STMicroelectronics.X-CUBE-TOUCHGFX.4.15.0 Mode and configuration.

AGendrau
Associate

When Graphics Application is checked, a folders tree starting from TouchGFX, with files like GFX2.touchgfx, etc, is generated. It’s OK.

When the .ioc file becomes complicated (as the example I attach), it seems that TouchGFX is replaced by Src and all files are generated under Src, mixing them with main.c and the other files.

Could you fix this, please?

1 REPLY 1
Patrizia BELLITTO
ST Employee

Hello,

sorry but this is not the correct category for this question...please, try to move it under STM32 Q&A pages.

Regards,

Patrizia