Other: software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to download STSW-WPSTUDIO

Hello, I bought a STWLC38 evaluation board and I need to install STSW-WPSTUDIO for adjusting and configuring the board. While I'm trying to download the software, it shows error "This software is not available for download." Can somebody help me to e...

Capture.PNG

USB Power Delivery using STUSB1602 library

Hi there,We are using the STUSB1602 for charging 10W devicesI'm looking to download the STSW-STUSB010 library, It seams that the STSW-STUSB010 library is not available, also from web search, there is version 015  some sites claim that the library is ...

GalBTM by Associate II
  • 681 Views
  • 1 replies
  • 0 kudos

L6470

Hi,I am usinga) L6470 to control Stepper motors. I am using STP-MTR-23079(x). The motor has rated current=2.8A/phase, Resisteance=1.1ohm/phase.b) I am using 24VDC for L6470.c) I am setting KVAL = 14.04% with phase current that is around 3.07A/phase. ...

CSu.12 by Associate II
  • 627 Views
  • 0 replies
  • 0 kudos