2008-05-09 06:47 PM
Very Crucial!!! Running Bootloader from Bank1 and also Switching
2011-05-17 12:53 AM
Folks,
I need an immediate response (very clear steps) for IAR 5.11 WorkBench IDE environment with respect two problems I am facing. 1) The bootloader program working on Bank0 is unable to come in Bank 1 (since running in release mode here, is it necessary that we need to run in release mode here??). I get some kind of stack flow error due to which unable to go to main, Also ARM error Core Id (0x00000) kind of error also when I try to run tbe bootloader bank1. 2) Second Problem is once I could run the Bootloader from Bank1, then comes with other problem how to switch between Bank1 and Bank0. What mistakes are we taking care here? Give very clear clear instructions. 2)