Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can STCC2540 be used in a USB OTG scenatio?

My system is OTG capable- means it can work in Host as well as device mode. The use case is that my system should be able to connect to mobiles and tabs where they are client devices and I should be able to charge them, also being a USB host. Also my...

Resolved! M24512-A125 EEPROM memory address write cycles

Hello,I am a developer making a product that controls the M24512-A125 EEPROM with I2C.I am positive about the M24512-A125 product.I have a question while developing.I know there is a limit to the write cycles.Please let me know if my analysis is corr...

0693W00000D05KmQAJ.png
Skim.3 by Associate
  • 887 Views
  • 1 replies
  • 0 kudos

Hi, Was planning to implement a design based on STUSB4500. have some queries about the working of STUSB4500 under different conditions.

1. If we are using A_B_Side for Super speed MUX selection, whether this A_B_side will be available on followinga) if a USB2.0 or Type A connected to Type C port using a USB2.0 or Type A to Type C connector.b)Whether ATTACH or A_B_Side is suitable for...

AV.6 by Associate II
  • 734 Views
  • 1 replies
  • 0 kudos

STM32F4 - Radiolink SE100 GPS

Hi. I am using STM32F407VGT6 this one and RadioLink SE100 GPS. I am trying to get $GNGGA data via USART and displaying it in putty terminal. I am able to get and print data. After 3-4 minutes gps sensor led is blinking but no data is printed on termi...

JMohn.1 by Associate
  • 1373 Views
  • 1 replies
  • 0 kudos

Invalid File Format

I'm trying to edit a power supply design project that I just recently worked on. However, when I try to open it I get an "Invalid File Format" error. Any idea how to fix this?

PGyur.1 by Associate II
  • 1727 Views
  • 5 replies
  • 0 kudos