cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-MKI228KA arduino

ljm
Associate III

Hello,

Please , can i use the module STEVAL-MKI228KA (ILPS22QS) with arduino ?

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @ljm ,

Yes you can.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @ljm ,

Yes you can.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@ljm wrote:

can i use the module STEVAL-MKI228KA (ILPS22QS) with arduino ?


Of course you can: the sensor neither knows nor cares what microcontroller or software framework you use - all it needs to see is valid signals at its pins.

The only thing to beware of would be voltage levels - are you using a 5V or 3V Arduino?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.