cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with Getting Started Application b/w X-NUCLEO-GNSS and B-L475e-IOT01A1. No previous connection to the Internet is done by the B-L475e-IoT node.

MChav.13
Associate II

The guide/documentation provided talks mainly b/w the X-NUCLEO-GNSS sensor and a NUCLEO board while I am attempting to use the L475e-IoT Node. When interacting with the application on Tera Term, the menu from the example is displayed. However, when asking to display a "position" the screen displays: "Last position wasn't valid." Moreover, the documentation requests that your IoT Node should be connected to the Internet but when rebooting the IoT Node board it never looks for a WiFi spot to connect to rather it just goes straight into the GNSS application example.

Any further directions, tips, or tutorials will be highly appreciated.

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @MChav.13​ , I suggest you to share this topic in the STM32 community for the STM32L4 help and Interface And Connectivity ICs for RF and BLE support. Regards

Thank you Eleon. I will do so.