2019-07-12 02:13 PM
The guide/documentation provided talks mainly b/w the X-NUCLEO-GNSS sensor and a NUCLEO board while I am attempting to use the L475e-IoT Node. When interacting with the application on Tera Term, the menu from the example is displayed. However, when asking to display a "position" the screen displays: "Last position wasn't valid." Moreover, the documentation requests that your IoT Node should be connected to the Internet but when rebooting the IoT Node board it never looks for a WiFi spot to connect to rather it just goes straight into the GNSS application example.
Any further directions, tips, or tutorials will be highly appreciated.
2019-07-15 04:05 AM
Hi @MChav.13 , I suggest you to share this topic in the STM32 community for the STM32L4 help and Interface And Connectivity ICs for RF and BLE support. Regards
2019-07-16 06:46 PM
Thank you Eleon. I will do so.