Official library for LIS3DH with FIFO DMA transfer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-08 7:49 AM
HI, I am trying to develop a application with a accelerometer over 5kHz.
I have some samples of LIS3DH. Does exits any repository of mem senc?
I search in cubemx but is not there.
I can write the library from datasheet but it is a lot of time and it will not be mantain.
do you know if other device in cubemx or in c official library is supported by st?
I am interested on fifo DMA transfer by I2c .
Thanks fot all, tcg
- Labels:
-
DMA
-
I2C
-
STM32CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-08 2:17 PM
It's just I2C transfer. Can't you do anything yourself instead of just library&cut&paste?
PS. Works perfect. i used LIS3DH
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-08 11:47 PM
yes of course, but as I said, I would prefer to know if there is an official library for maintenance and integration.
Kind regards, tcg
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-09 4:04 AM
Hi @Tomás Cabeza​ ,
There is a C example for FIFO configuration on LIS3DH on Github, you can find it at this link --> lis3dh_multi_read_fifo.c.
Then once you have the data from the FIFO, you can implement the DMA transfer through STM32 / CubeMX libraries.
-Eleon
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-09 4:40 AM
Thanks a lot @Eleon BORLINI​ .
I will try this code tomorrow. I will give you a feedback
Thanks a lot for your fast response, tcg
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-10 6:53 AM
HI @Eleon BORLINI​
That works, 1) I have just understand that DMA have no sense with I2C becouse a fifo reading for 192 bytes is the same, is not it?
is it possible create a dma for this? The difference iss that the processor is free during the i2c transaction.
I am trying to make a i2c reading of 192 i2c after int1 event is detected. That event could be with ov or watermaker 2/3 fifo.Is that correct?
2) LIS3DH is not real 5kHz Bw is only OutputSR. Does it exits any device in st roadmap with (>3-4kHz BW) >OSR?
kind regards, tcg
2)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-10 8:29 AM
​ Hi @Eleon BORLINI​
That seems that work well.
But I am not able to control the INT1 with watermark o ov fifo. Any idea?
It is a little spaguetti code...
Thanks for all.
-----
/* Initialize mems driver interface */
stmdev_ctx_t lis3dh_ctx;
lis3dh_ctx.write_reg = platform_write;
lis3dh_ctx.read_reg = platform_read;
lis3dh_ctx.handle = &SENSOR_BUS;
lis3dh_reg_t LIS3DH_reg;
/* Check device ID */
lis3dh_device_id_get(&lis3dh_ctx, &whoamI);
/* Enable Block Data Update */
lis3dh_block_data_update_set(&lis3dh_ctx, PROPERTY_ENABLE);
//CTRL_REG1 (20h)
// ODR [3:0] -> Set Output Data Rate
lis3dh_data_rate_set(&lis3dh_ctx, LIS3DH_ODR_5kHz376_LP_1kHz344_NM_HP );
/* Set operating mode to high resolution */
lis3dh_operating_mode_set(&lis3dh_ctx, LIS3DH_LP_8bit);
//CTRL_REG2 (21h)
//HPM[1:0] High-pass filter mode selection. Default value: 00Refer to Table 34: High-pass filter mode configuration
//HPCF[2:1] High-pass filter cutoff frequency selection
//FDS Filtered data selection. Default value: 0 (0: internal filter bypassed; 1: data from internal filter sent to output register and FIFO)
//HPCLICK High-pass filter enabled for CLICK function.(0: filter bypassed; 1: filter enabled)
//HP_IA2 High-pass filter enabled for AOI function on interrupt 2, (0: filter bypassed; 1: filter enabled)
// HP_IA1 High-pass filter enabled for AOI function on interrupt 1, (0: filter bypassed; 1: filter enabled)
uint8_t high_pass_on_outputs_value;
lis3dh_high_pass_on_outputs_get(&lis3dh_ctx,&high_pass_on_outputs_value);
//CTRL_REG3 (22h)
LIS3DH_reg.ctrl_reg3.i1_321da=0;
LIS3DH_reg.ctrl_reg3.i1_click=0;
LIS3DH_reg.ctrl_reg3.i1_ia1=0;
LIS3DH_reg.ctrl_reg3.i1_ia2=0;
LIS3DH_reg.ctrl_reg3.i1_overrun=1; // FIFO overrun interrupt on INT1. 1: enable
LIS3DH_reg.ctrl_reg3.i1_wtm=1; // FIFO watermark interrupt on INT1. 1: enable
LIS3DH_reg.ctrl_reg3.i1_zyxda=0;
lis3dh_pin_int1_config_set(&lis3dh_ctx,&LIS3DH_reg.ctrl_reg3);
//CTRL_REG4 (23h)
// FS[1:0] Full-scale selection. (00: ±2 g; 01: ±4 g; 10: ±8 g; 11: ±16 g)
lis3dh_full_scale_set(&lis3dh_ctx, LIS3DH_2g);
//HR High-resolution output mode (0: high-resolution disabled; 1: high-resolution enabled)
// FIFO
lis3dh_op_md_t mode;
lis3dh_operating_mode_get(&lis3dh_ctx, &mode);
/* Set FIFO watermark to 25 samples */
lis3dh_fifo_watermark_set(&lis3dh_ctx, 25);
int8_t watermark;
lis3dh_fifo_watermark_get(&lis3dh_ctx, &watermark);
//FIFO_CTRL_REG (2Eh)
// FM -> Set FIFO mode to Stream mode: Accumulate samples and override old data */
lis3dh_fifo_mode_set(&lis3dh_ctx, LIS3DH_DYNAMIC_STREAM_MODE); //LIS3DH_STREAM_TO_FIFO_MODE
//TR -> Trigger selection; 0: Int1, 1: Int2
lis3dh_fifo_trigger_event_set(&lis3dh_ctx,LIS3DH_INT1_GEN);
lis3dh_tr_t INT_Selected;
lis3dh_fifo_trigger_event_get(&lis3dh_ctx,&INT_Selected);
//CTRL_REG5 (24h)
//FIFO_EN
lis3dh_fifo_set(&lis3dh_ctx, PROPERTY_ENABLE);
//INT_POLARITY INT1 and INT2 pin polarity. Default value:
//lis3dh_read_reg(&dev_ctx,0,&LIS3DH_reg);
lis3dh_ble_t dataformat_value;
lis3dh_data_format_get(&lis3dh_ctx,&dataformat_value);
// Disable all interrupt events from x,y,z
//INT1_SRC (31h)
LIS3DH_reg.int1_cfg._6d=0;
LIS3DH_reg.int1_cfg.aoi=1;
LIS3DH_reg.int1_cfg.xhie=0;
LIS3DH_reg.int1_cfg.xlie=0;
LIS3DH_reg.int1_cfg.yhie=0;
LIS3DH_reg.int1_cfg.ylie=0;
LIS3DH_reg.int1_cfg.zhie=0;
LIS3DH_reg.int1_cfg.zlie=0;
lis3dh_int1_gen_conf_set(&lis3dh_ctx, &LIS3DH_reg.int1_cfg);
lis3dh_int1_gen_conf_get(&lis3dh_ctx, &LIS3DH_reg.int1_cfg);
//INT2_CFG (34h)
LIS3DH_reg.int2_cfg._6d=0;
LIS3DH_reg.int2_cfg.aoi=1;
LIS3DH_reg.int2_cfg.xhie=0;
LIS3DH_reg.int2_cfg.xlie=0;
LIS3DH_reg.int2_cfg.yhie=0;
LIS3DH_reg.int2_cfg.ylie=0;
LIS3DH_reg.int2_cfg.zhie=0;
LIS3DH_reg.int2_cfg.zlie=0;
lis3dh_int2_gen_conf_set(&lis3dh_ctx, &LIS3DH_reg.int2_cfg);
lis3dh_int2_gen_conf_get(&lis3dh_ctx, &LIS3DH_reg.int2_cfg);
//INT2_SRC (35h) -> interrupt state
//INT2_THS (36h) -> level of mg event
//INT2_DURATION (37h)-> event duration
while (1)
{
lis3dh_fifo_status_get(&lis3dh_ctx, &LIS3DH_reg.fifo_src_reg);
if (LIS3DH_reg.fifo_src_reg.ovrn_fifo==1){
lis3dh_int1_gen_conf_get(&lis3dh_ctx, &LIS3DH_reg.int1_cfg);
platform_delay(2);
lis3dh_fifo_status_get(&lis3dh_ctx, &LIS3DH_reg.fifo_src_reg);
}