Associate II
December 23, 2022
Solved
Use a function from library
- December 23, 2022
- 3 replies
- 3201 views
Hello!
I am working on a project of sound source localization and want to lit an individual ws2812 Led in the direction of the sound source.
I came across an expansion software package x-cube-memsmic1 which uses Acoustic SL library to estimate the angle of the sound source and send the angle along with some other things to PC via USB. The description says that the audio_application.c and usbd_audio_if.c contains some functions to get the angle from the source and send it.
Now I don't know which function does this and how?
/**
******************************************************************************
* @file audio_application.c
* @author SRA
* @version v1.3.0
* @date 17-Sep-2021
* @brief Source localization example.
******************************************************************************
* @attention
*
* Copyright (c) 2022 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "audio_application.h"
#include "acoustic_sl.h"
/** @addtogroup X_CUBE_MEMSMIC1_Applications
* @{
*/
/** @addtogroup ACOUSTIC_SL_Example
* @{
*/
/** @defgroup AUDIO_APPLICATION
* @{
*/
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/** @defgroup AUDIO_APPLICATION_Exported_Variables
* @{
*/
uint16_t PDM_Buffer[((((AUDIO_IN_CHANNELS * AUDIO_IN_SAMPLING_FREQUENCY) / 1000) * MAX_DECIMATION_FACTOR) / 16)* N_MS ];
/**
* @}
*/
/** @defgroup AUDIO_APPLICATION_Private_Variables
* @{
*/
/* Private variables ---------------------------------------------------------*/
/*Handler and Config structure for Source Localization*/
AcousticSL_Handler_t libSoundSourceLoc_Handler_Instance;
AcousticSL_Config_t libSoundSourceLoc_Config_Instance;
volatile int16_t SOURCE_Angle_Value = 0;
volatile uint16_t SOURCE_Enable_Value = 1;
extern UART_HandleTypeDef UartHandle;
volatile int32_t result[2];
static uint16_t PCM_Buffer[AUDIO_IN_CHANNELS * AUDIO_IN_SAMPLING_FREQUENCY / 1000];
/**
* @}
*/
/** @defgroup AUDIO_APPLICATION_Exported_Function
* @{
*/
/**
* @brief Half Transfer user callback, called by BSP functions.
* @param None
* @retval None
*/
void CCA02M2_AUDIO_IN_HalfTransfer_CallBack(uint32_t Instance)
{
UNUSED(Instance);
AudioProcess();
}
/**
* @brief Transfer Complete user callback, called by BSP functions.
* @param None
* @retval None
*/
void CCA02M2_AUDIO_IN_TransferComplete_CallBack(uint32_t Instance)
{
UNUSED(Instance);
AudioProcess();
}
/**
* @brief User function that is called when 1 ms of PDM data is available.
* In this application only PDM to PCM conversion and USB streaming
* is performed.
* User can add his own code here to perform some DSP or audio analysis.
* In this case audio libraries are used
* @param none
* @retval None
*/
void AudioProcess(void)
{
if (CCA02M2_AUDIO_IN_PDMToPCM(CCA02M2_AUDIO_INSTANCE, (uint16_t *)PDM_Buffer, PCM_Buffer) != BSP_ERROR_NONE)
{
Error_Handler();
}
if (AcousticSL_Data_Input((int16_t *)&PCM_Buffer[BOTTOM_LEFT_MIC], (int16_t *)&PCM_Buffer[TOP_RIGHT_MIC],
(int16_t *)&PCM_Buffer[BOTTOM_RIGHT_MIC], (int16_t *)&PCM_Buffer[TOP_LEFT_MIC], &libSoundSourceLoc_Handler_Instance) == 1U)
{
SW_Task2_Start(); /*Localization Processing Task*/
}
Send_Audio_to_USB((int16_t *)PCM_Buffer, AUDIO_IN_SAMPLING_FREQUENCY / 1000 * AUDIO_IN_CHANNELS);
}
/**
* @brief Initialize the audio libraries adopted
* @param None
* @retval None
*/
void Audio_Libraries_Init(void)
{
__IO uint32_t error_value = 0;
/* Enable CRC peripheral to unlock the library */
__CRC_CLK_ENABLE();
/*Setup Source Localization static parameters*/
libSoundSourceLoc_Handler_Instance.channel_number = 4;
libSoundSourceLoc_Handler_Instance.M12_distance = DIAGONAL;
libSoundSourceLoc_Handler_Instance.M34_distance = DIAGONAL;
libSoundSourceLoc_Handler_Instance.sampling_frequency = AUDIO_IN_SAMPLING_FREQUENCY;
libSoundSourceLoc_Handler_Instance.algorithm = ACOUSTIC_SL_ALGORITHM_GCCP;
libSoundSourceLoc_Handler_Instance.ptr_M1_channels = 4;
libSoundSourceLoc_Handler_Instance.ptr_M2_channels = 4;
libSoundSourceLoc_Handler_Instance.ptr_M3_channels = 4;
libSoundSourceLoc_Handler_Instance.ptr_M4_channels = 4;
libSoundSourceLoc_Handler_Instance.samples_to_process = 512;
(void)AcousticSL_getMemorySize(&libSoundSourceLoc_Handler_Instance);
libSoundSourceLoc_Handler_Instance.pInternalMemory = (uint32_t *)malloc(libSoundSourceLoc_Handler_Instance.internal_memory_size);
error_value += AcousticSL_Init(&libSoundSourceLoc_Handler_Instance);
/*Setup Source Localization dynamic parameters*/
libSoundSourceLoc_Config_Instance.resolution = 10;
libSoundSourceLoc_Config_Instance.threshold = 24;
error_value += AcousticSL_setConfig(&libSoundSourceLoc_Handler_Instance, &libSoundSourceLoc_Config_Instance);
/*Error Management*/
if (error_value != 0U)
{
Error_Handler();
}
/*Malloc Failure*/
if (libSoundSourceLoc_Handler_Instance.pInternalMemory == NULL)
{
Error_Handler();
}
}
/**
* @brief Initializes two SW interrupt with different priorities
* @param None
* @retval None
*/
void SW_IRQ_Tasks_Init(void)
{
HAL_NVIC_SetPriority((IRQn_Type)EXTI1_IRQn, 0x0D, 0);
HAL_NVIC_EnableIRQ((IRQn_Type)EXTI1_IRQn);
HAL_NVIC_SetPriority((IRQn_Type)EXTI2_IRQn, 0x0E, 0);
HAL_NVIC_EnableIRQ((IRQn_Type)EXTI2_IRQn);
}
/**
* @brief Highest priority interrupt handler routine
* @param None
* @retval None
*/
void SW_Task1_Callback(void)
{
}
/**
* @brief Lower priority interrupt handler routine
* @param None
* @retval None
*/
void SW_Task2_Callback(void)
{
(void)AcousticSL_Process((int32_t *)&result, &libSoundSourceLoc_Handler_Instance);
if (result[0] == ACOUSTIC_SL_NO_AUDIO_DETECTED)
{
result[0] = -1;
}
if (result[0] != -1)
{
char output[4];
int32_t n = sprintf(output, "%li", (int32_t)result[0]);
(void)HAL_UART_Transmit(&UartHandle, (uint8_t *)" ", 4, 0xFFFF);
(void)HAL_UART_Transmit(&UartHandle, (uint8_t *)"\r", 1, 0xFFFF);
(void)HAL_UART_Transmit(&UartHandle, (uint8_t *)output, (uint16_t)n, 0xFFFF);
}
}
/**
* @brief Throws Highest priority interrupt
* @param None
* @retval None
*/
void SW_Task1_Start(void)
{
HAL_NVIC_SetPendingIRQ(EXTI1_IRQn);
}
void SW_Task2_Start(void)
{
HAL_NVIC_SetPendingIRQ(EXTI2_IRQn);
}
void Error_Handler(void)
{
while (1);
}
/**
* @}
*/
/**
* @}
*/
/**
* @}
*/
/**
* @}
*/Can someone tell me how can I get that specific function so I can put it in main loop?
Thanks
Viki