2023-11-13 12:27 AM
Hello,
I have question please, can you tell me the protection index (IP) of the LPS28DFW ?
also the LPS22DF has 22000g High shock survivability, it's perfromant for my application but for the LPS28DFW i don't find any information on the datasheet about the High shock survivability.
Can you tell me if the 2 sensors have the same High shock survivability or not ?
Thank you very much
2023-11-10 2:52 AM
Hello,
I have question please, can you tell me the protection index (IP) of the LPS28DFW ?
also the LPS22DF has 22000g High shock survivability, it's perfromant for my application but for the LPS28DFW i didn't found any information in the datasheet about the High shock survivability.
Can you tell me if the 2 sensors have the same High shock survivability or not ?
Thank you very much
2023-11-16 7:44 AM
Hi @ljm ,
If it is not written on the datasheet, there is no IP certification.
By construction and package closure, the 28DFW is more robust than the 22DF and therefore has a higher high shock survivability than 22000g.
2023-11-17 4:50 AM
thank you very much for your feedback.
from what i've seen the price of the lps28dfw is almost 2 to 3 times more expensive than the lps22df.
is this difference explained by the advantage of the LPS28DFW which has a fairly high measuring range and the added gel for waterproofing ?
One last question please, for the LPS28DFW's dust tightness, can you recommend any of your products that might help me ? and thank you.
2023-11-20 4:41 AM
thank you very much for your feedback.
from what i've seen the price of the lps28dfw is almost 2 to 3 times more expensive than the lps22df.
is this difference explained by the advantage of the LPS28DFW which has a fairly high measuring range and the added gel for waterproofing ?
One last question please, for the LPS28DFW's dust tightness, can you recommend any of your products that might help me ? and thank you.
2023-11-22 1:40 AM
Hi @ljm ,
For dust, LPS28DFW is more immune due to the presence of gels, while dust on LPS22DF could alter the measurement by closing the holes where the pressure is read.
2023-11-22 4:38 AM
Thank you for your reply.
Does this mean that the existing gel on the LPS28DFW protects against water and dust at the same time? Because the environment where the sensor is used, there is too much dust? Do you have any idea if the existing gel on the LPS28DFW protects against large dust (in mm) or even for small dust (in micro-meter)?
2023-11-22 8:01 AM
hello @Federica Bossi
because as far as I know, dust can accumulate on the gel.
2024-01-19 1:00 AM
hello @Federica Bossi
For the LPS22DF, LPS27HW and LPS28DFW, i need to know the response time, means the necessary time to mesure the pressure.
Thank you very much