cancel
Showing results for 
Search instead for 
Did you mean: 

How to fine tune STHS34PF80 effective presence detection range ?

SLin.11
Associate III

Hi All,

I started with example to make STHS34PF80 presence detection working.

Now I tried to add effective presence detection range.

Where should I start ? Is there a suggested process ?

 

 

3 REPLIES 3
Federica Bossi
ST Employee

Hi @SLin.11 ,

You can find some examples on github, let me know if this helps :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

My existing code is based on this example, however the presence detection range is around 1.2 meters.

I want to extend the range up to 2.5~3 meters however there is no criteria in example what parameters to tune.

 

 

Federica Bossi
ST Employee

Hi @SLin.11 ,

You can detect the presence at higher distance changing the threshold. Keep in mind that the sensor must be tuned based on the application and the environmental conditions. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.