2024-01-17 12:58 AM
Hi All,
I started with example to make STHS34PF80 presence detection working.
Now I tried to add effective presence detection range.
Where should I start ? Is there a suggested process ?
2024-01-18 12:22 AM
2024-01-18 12:57 AM
My existing code is based on this example, however the presence detection range is around 1.2 meters.
I want to extend the range up to 2.5~3 meters however there is no criteria in example what parameters to tune.
2024-02-01 5:31 AM
Hi @SLin.11 ,
You can detect the presence at higher distance changing the threshold. Keep in mind that the sensor must be tuned based on the application and the environmental conditions.