2020-11-10 12:13 AM
Hi,
my goal is to use custom template files in AlgoBuilder. For instance have an extra function or class in the main.c file. Therefore I would like to create a new firmware template for NUCLEO-L476RG as described in en.UM2689.
I am working with CubeMX, since in CubeIDE it is not possible to change the "application structure" to "Basic".
I am following the description in en.UM2689, setting the application to "IKS01A3_AlgoBuilder_Template", etc. After generating the code, I copy the whole project location to C:\Users\USER_NAME
\STMicroelectronics\AlgoBuilder\FirmwareTemplate\.
Then I restart Algobuilder and try to create a new design for the new target. However, the new target is not available in the dropdown list as shown on Figure 29.:
Is there anything, I am missing? If I go to C:\Program Files (x86)\STMicroelectronics\AlgoBuilder\ProjectTemplate, I see a target.xml file describing different targets.
Solved! Go to Solution.
2020-11-11 2:51 AM
Hi Miroslav,
I have definitely made some progress:
Here I have some problems. I am looking at the file "algo_builder.c" from the template and compare it to the C code which is shown. I would accept, that they are the same, but it is not the case. Should they be the same or do I misunderstand something at concept level.
I am going to send you:
Thank you for your help!
Best regards,
Attila
2020-11-10 1:50 AM
Hi,
did you select the Toolchain/IDE in the Firmware settings first?
If yes, can you please share with me your Project Template so I can test it?
2020-11-10 2:10 AM
2020-11-10 2:11 AM
2020-11-11 12:26 AM
HI,
I have checked your project.
1) For STM32CubeIDE you have to uncheck the Generate Under Root option in Project Manager tab. The project files must be inside STM32CubeIDE directory.
2) I see peripherals (TIM, CRC, I2C) are not configured as it is described in the UM2689.
2020-11-11 2:51 AM
Hi Miroslav,
I have definitely made some progress:
Here I have some problems. I am looking at the file "algo_builder.c" from the template and compare it to the C code which is shown. I would accept, that they are the same, but it is not the case. Should they be the same or do I misunderstand something at concept level.
I am going to send you:
Thank you for your help!
Best regards,
Attila
2020-11-11 2:56 AM
2020-11-12 12:25 AM
Hi Attila
your latest template seems to be fine. I have tested it quickly and it works.
algo_builder.c is generated by the AlgoBuilder application according to your design, so it wont be the same as it is in the template.
2020-11-13 3:53 AM
Hi Miroslav,
thank you for your support. Everything works fine. We are experimenting with our own blocks based on templates right now. It is super cool!
Best regards,
Attila