Hello @Apollo1 the MEMS Studio opens the serial port and send "CMD_Read_PresString" command to read presentation string. This string describes the firmware and MEMS Studio can adjust the GUI according to the connected firmware.The firmware from X-CUB...
Hello @Apollo1,Usually this kind of issue is caused by the firmware which is not working properly due to incorrect configuration in CubeMX.Can you share your project and/or .ioc file. I can check it.
Hello @tarunprasadoff The NUCLEO (STM32) must be programmed with compatible firmware with MEMS Studio.You can check chapter 2.6 Hardware and firmware compatibility in UM3233.NUCLEO-L476RG + X-NUCLEO-IKS4A1 can be used in AlgoBuilder in MEMS Studio.Se...
Hello @Frabbit these are not errors but only warnings due to more strict gcc compiler. The binary file is generated and you can program the Sensortile.box.