2017-07-17 5:12 AM
I bought the
STEVAL-FKI868V1
development kit and when I try to open the COM port on the GUI, I get the following error message:''Wrong FW in the Selected Board''. I go to the Binary folder in the application program files and I drag and drop the SIGFOX_CLI_DEMO_NUCLEO_L1_ETSI.bin file to the mbed drive and press the reset button. I try to open the COM port again in the GUI, and the same error message appears. There's nothing on the serial port as well on my terminal when I reset the board. Are there any extra steps which need to be taken before trying to open the port?
Any assistance would be appreciated.
Nitesh Reddy
2018-04-17 2:45 AM
Hello,
I have the same pb but i was not able to find the
SIGFOX_CLI_DEMO_NUCLEO_L1_ETSI.bin
Could you tell me where you found it so that i try and let you know if i still have the pb
Regards
2018-05-09 3:14 PM
Firmware is stored in 'C:\Program Files (x86)\STMicroelectronics\S2-LP_SigFox_DK_1.3.0\Binary' or similar folder, depending on the software version. It seems they are the same for FCC and ETSI now.
2018-05-09 9:24 PM
Yes. In the latest DK, it supports different zones with the same library.
Please choose MCU accordingly. Currently F0, F4, L0, L1 are available.
2018-05-22 1:36 PM
Hello, Winfred. I'm having the same problem and I have tried everything and nothing works.
Please I need some help! I have the development of the Bluenrg2 which is the steval IDB008V2 and the steval FKI868V1.
I made the hardware modifications so that the steval FKI868V1 can be compatible with the steval IDB008V2 (bluenrg 2), I set the antenna, and I tried to flash the binary files F0, F4, L0, L1, and connect with the COM port. But unfortunately, none didn't work!!! I got the same message 'Wrong firmware... Please flash the correct firmware' in the GUI. What's going on? I don't understand!! Please I need your help, this is very important for a project that I'm working with... I'm desperate, I don't know what to do.
2018-05-23 2:44 AM
Hi Johan,
STSW-BNRG-S2LP is the kid you need to test BlueNRG1/2 with S2-LP for Sigfox applications.
Please download from:
Please try the prebuild FW located:
C:\Program Files (x86)\STMicroelectronics\BLE-Sub1GHz DK_1.0.0\Firmware\BLE_SigFox_SensorDemo\
The FW shall be working with your IDB008v2+FKI868V1.
It sends a Sigfox frame (containing a four byte counter) whenever the button_2 is pressed.
Please note that HW modification on IDB008V2 is required.
Please refer to UM2211 for details:
http://www.st.com/resource/en/user_manual/dm00390265.pdf
-----
This would be a different problem actually.
Please if possible create a new thread for different issues, so that it will be easier for other people to search.Thank you.
Best Regards,
Winfred