Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L4CD / VL53L0X wavelength detection

Dear all,I'm working on a product where we use 850 nm LEDs with a typical spectrum like shown below:Since we emit quite some light (10's of Watts in short, ms bursts) with our device in a narrow cone (about the same FOV as the ST sensors), I'm wonder...

TH3_0-1728286469102.png
TH3 by Associate II
  • 2031 Views
  • 3 replies
  • 0 kudos

VL53L8CX with stm32f407vgt6

I am trying to use VL53l8cx with STM32F407VGT6 to find depth . I have previously worked with VL53l5cx and VL53l1cx  and was comfortab;e with both of these .  I am unable to use this sensor at all as everytime a hard fault arises . I have been able to...

Rituraj_0-1728285114831.png
Rituraj by Senior
  • 1965 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L5CX/8CX LookUp-Table

Hi,i know that there are already a few posts on this topic, and i know the VL53L8CX has the same table as the VL53L5CX. But i just wanted to know, if anyboy could post the calculations for the LookUp-Table?Thanks!

Hartm_Sve by Associate II
  • 1391 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L0X determining small object is at fixed distance

HelloI need to trigger an action whenever a small object (aprox 1 cm diameter) is at a fixed distance (around 10 cm) of the sensor.Using VL53L0X the readings I get are very much affected by the background, for example if the object is in range and th...

oscar118 by Associate
  • 1976 Views
  • 2 replies
  • 0 kudos

Resolved! Measurement range of VD55H1

Dear Sir or Madam,what is the absolute minimum measurement distance of VD55H1 3D iToF sensor die?Could you provide a (detailed) datasheet and application notes? Currently, there is only a data brief. Best regardsLukas Bath

Resolved! Clarification on Time-of-Flight Cover Glass

Hi,  I was reading @John E KVAM excellent post on Time of flight sensor glass:https://community.st.com/t5/mems-and-sensors/time-of-flight-cover-glass/ta-p/49259and this documentationhttps://www.st.com/content/ccc/resource/technical/document/applicati...

J1234_0-1727837224035.png J1234_1-1727837305511.png
J1234 by Associate
  • 1255 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CX IO

 Hi Team, We are using the VL53L4CX in QCS8550 platform.Below are queries listed below for clarification. Query 1:Load Capacitance I'm using a same I2C for 5 sensors of VL53L4CX. Is that good to connect or any load capacitance issues will occur Need ...

VL53L8CX motion detection

Hi! I am trying to use motion detection data from VL53L8CX sensor. Where can I find deeper explanation of results data and configuration structure than is it in datasheets.RESULTSstruct{uint32_t global_indicator_1;uint32_t global_indicator_2;uint8_t ...

MSkrt by Associate II
  • 1798 Views
  • 1 replies
  • 0 kudos