Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STEVAL-CAM-M0I Pinout compatibility with Raspberry Pi CM4

Hi, we are using the STEVAL-CAM-M0I board to evaluate the 55G0 protomodule.I have it connected to a raspberry pi CM4 IO breakout board, to the CAM1 CSI-2 interface.There is a provided driver, etc for this from ST, but it appears the pinout is not 1:1...

Bryan1986_0-1729091639422.png Bryan1986_1-1729091755751.png
Bryan1986 by Associate II
  • 3215 Views
  • 5 replies
  • 2 kudos

Resolved! VL53L1 Dynamic SPAD Selection Question

Hi!I have two short questions regarding the dynamic SPAD selection happening on the VL53L1 sensor discussed previously here:- Is there a minimum number of SPADs after the selection? As in, by utilizing a 4x4 region, should I expect no oscillations (t...

LDMigotto by Associate II
  • 1759 Views
  • 1 replies
  • 1 kudos

Resolved! vl53l1x number of SPAD?

I have been using GetResult method of grabbing the sensor reading.  It returns this structure: typedef struct {uint8_t Status; /*!< ResultStatus */uint16_t Distance; /*!< ResultDistance */uint16_t Ambient; /*!< ResultAmbient */uint16_t SigPerSPAD;/*!...

will3 by Associate III
  • 1286 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1 Water level measurement incorrect values

Hello.I’m utilizing the VL53L1 sensor to measure water level inside of a closed water bucket.While using a 30cm tall white bucket half full, with the VL53L1 positioned at the top aiming down at the air-water interface, the sensor sometimes outputs in...

LDMigotto by Associate II
  • 7487 Views
  • 7 replies
  • 4 kudos

Resolved! Using ToF sensor to measure distance to small object

Hello,Basically i am trying to measure distance to a hand that moves above the sensor, returned distance is used to light leds approximately at hand height. My problem is that hand is probably to small object or its reflectivity is not enough that ab...

pasikav by Associate
  • 1896 Views
  • 1 replies
  • 1 kudos

VL53L4CD / VL53L0X wavelength detection

Dear all,I'm working on a product where we use 850 nm LEDs with a typical spectrum like shown below:Since we emit quite some light (10's of Watts in short, ms bursts) with our device in a narrow cone (about the same FOV as the ST sensors), I'm wonder...

TH3_0-1728286469102.png
TH3 by Associate II
  • 2017 Views
  • 3 replies
  • 0 kudos