2024-06-23 11:28 PM
Hi,
2024-07-02 04:56 PM
2024-07-08 07:53 AM
This is a little tricky. One has to compile a library not for 'android' or 'linux' but for the particular CPU (or MCU). Our existing libraries are for Arm Cortex processors - because that's what the STM32 is based on. If you want a different CPU, one pretty much as to specify which CPU it is.
It's also tricky because unless someone has to dig up a cross-compiler. Not impossible, but not easy either.
2024-07-09 12:47 AM
Hello,
The libraries were added on st.com in the STSW-IMG048 revision 1.0.1
You can find them in the SmartPresenceDetectionKit_LnA_1.0.0 direcotry.