Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SmartPresenceDetectionKit_LnA_1.0.0 on raspberry pi

HiI am trying to use this on a raspberry pi4 running ubuntu 2404. I am able to run make successfully but on trying to run the generated binary I get./spdkit error while loading shared libraries: /lib/aarch64-linux-gnu/libc.so: invalid ELFI don't know...

nickw by Associate
  • 3036 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L8CH histogram extraction with multiple configurations

I'm extracting the histogram data from the VL53L8CH. In the 8x8 mode, we are limited to few bins (~18) per reading. Is there a way to configure the sensor to oscillate the starting bin configuration so that I can get better range with the same bin pr...

wsun by Associate
  • 1242 Views
  • 2 replies
  • 2 kudos

Resolved! VL53L5CX address changes not working.

I am trying to run multiple VL53L5CX-TOF-sensors with a single Pi Pico to be able to stitch together multiple of the sensor images.However for this to work I have to change the i2c addresses of the sensors.I am trying to use the set_i2c_address funct...

FY by Associate
  • 1972 Views
  • 2 replies
  • 0 kudos

Resolved! Detect & correct for orientation of ToF Sensors

Hello,This is in regard to the question I posted at the webinar on AI-powered gesture recognition with Time-of-Flight sensors held on 3/11.  Can the orientation of the VL53L8CX ToF sensor be detected in case it is moved and possibly gets inverted aft...

BMcKnight by Associate II
  • 1704 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L4CX Histogram Data Interpreting

Hi! I've been testing the VL53L4CX sensor for the past few months and have finally decided to take a look at its additional histogram data. My most recent test is a measurement of an empty black bucket with a white sheet inside (to increase reflectiv...

LDMigotto by Associate II
  • 2773 Views
  • 2 replies
  • 1 kudos

Resolved! VL53L8CX ToF Sensor

Hi. I have question regarding VL53L8CX ToF sensor. The minimum distance is 2cm. The space between the objects being measured is less then that. Was wondering if it will be possible to reflect the light off from a mirror at 45 degrees to increase the ...

vl53L4CD GUI Not starting/opening

Hi,    i do not seem to be able to use the application gui for the vl53L4CD Nucleo board.    when i try and open the application i get this message. is anyone familiar with this issue?     

Afam_Nwokolo_0-1739982556393.png