Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L4CX - Drift on static level

Hello, I'm trying to measure a static level using the VL53L4CX. The following test shows an unusual drift in the level measured by the sensor. I'm using clean water for the test and a specific tank.I performed the test without any cover glass on the ...

Resolved! FDA accession number of the VL53L4CX

Hello,Do you have a FDA accession number for the VL53L4CX ToF chip? I can find only the document "VL53L4 IEC 60825-1 CB test certificate (eye safety)" at the attachments and there it isn't noted. Furthermore I guess it is not the same as for the VL53...

Tobias_1 by Associate
  • 941 Views
  • 1 replies
  • 0 kudos

Intefacing stmvl53l8cx with Cypress Cx3 controller

Hi @John E KVAM ,I am planning to interface stmvl53l8cx with cypress cx3 controller. I did not find any Register Reference for it to access the TOF registers. Instead I find  en.STSW-IMG042.zip SDK for raspberry pi . Should I port this SDK to my micr...

Vbala.1 by Associate II
  • 1753 Views
  • 4 replies
  • 1 kudos

Measuring liquid level in water bottle?

I came across STM's YouTube video demonstrating how to measure the level of a liquid inside a cup: https://www.youtube.com/watch?v=tHTNjmbO-GoI'd like to do something similar except for water bottles (of varying shapes, sizes, materials, and liquids)...

mattblee by Associate
  • 3219 Views
  • 2 replies
  • 2 kudos

Resolved! Have to reset power on VL53L4CX before code works again

Hi,I'm using an ESP32 (the RAK11200 module) with my own board (https://github.com/cyclops1982/TOFBoard/tree/main/TOFBoard).I'm using this helper file and basically do:1. A init() during the arduino setup()2. During the arduino loop() i run the GetDep...

cyclops by Associate III
  • 1318 Views
  • 2 replies
  • 1 kudos

Resolved! VL53L5CX Config error

I am trying to work with the VL53L5CX Tof sensor. The following calls succeed.VL53L5CX_InitVL53L5CX_ReadIDVL53L5CX_Start However, the following call fails:     VL53L5CX_Result_t pResult;    VL53L5CX_ProfileConfig_t _profile;    _profile.RangingProfil...

Resolved! X-CUBE-TOF1 with custom STM32H7 hardware

Hi all,I recently purchased an STM32H723VGT6 breakout board [https://github.com/WeActStudio/WeActStudio.MiniSTM32H723] (not a NUCLEO) and a VL53L5CX sensor breakout from Pololu [https://www.pololu.com/product/3417], and, as I'm a beginner and struggl...

hxtec32 by Associate II
  • 2816 Views
  • 3 replies
  • 0 kudos

Resolved! Build error for VL53L5CX on jetson nano, ubuntu

 Hi, I trying to using VL53L5CX with my jetson nano.Once I want to using it with arduino uno, but uno is not possibly for using with it.So I trying to connected directly it on my jetson. I'm trying to followingVL53L5CX_Linux manual that downloaded fr...

najon by Associate
  • 1212 Views
  • 2 replies
  • 0 kudos