Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cover glass for VL53L4ED

I am putting together a water level sensor based on the vl53l4ed. The device will be in an outdoors setting with wild swings in environmental conditions. I am having hard time to design a cover / cover glass system for the TOF sensor. I have now conc...

kossiN by Associate
  • 1314 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CD Setup Issue

Hello, Apologies in advance for the length of this post. I am looking for some advice as I am working on getting a cpp based callback for the VL53L4CD sensor, to do this I have written a file which should perform all the same setup as the driver prov...

BruGenie by Associate II
  • 1445 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L7CX et VL53L8CX

I recently purchased a VL53L7CX and VL53L8CX, so I wanted to test the Motion Indicator functionality for each zone to show if the targets moved and how they moved via SPD of the software by STM except that there, when two people present themselves in...

Freedy by Associate II
  • 3061 Views
  • 6 replies
  • 0 kudos

Resolved! Function of INT and SYNC in VL53L8CX

Hi Team,  Could you please share the detailed function of INT and SYNC in VL53L8CXV0GC/1?  We would probably use one sensor or two. If case of one sensor SYNC input doesn't add any value to the design. If two sensor used they'll probably share the pr...

Mukeshk by Associate II
  • 2602 Views
  • 7 replies
  • 1 kudos

Problem with TOF050C-VL6180X time-of-flight (TOF) sensors

Maybe someone can help me. I bought five TOF050C-VL6180X time-of-flight (TOF) sensors, which also work with the Adafruit_VL6180X library, but they behave completely differently:Two:At a distance of 30 mm, the script shows: 0 mmAt a distance of less t...

Jwinns by Associate
  • 1007 Views
  • 1 replies
  • 0 kudos

VL53L4CX - Temperature Issues (Drift)

Recently, I started a post about drift in the static level measurement using the VL53L4CX. I received some directions to continue the investigation, which I followed. I tested the performance by toggling the XSHUT pin as suggested, but it didn’t work...

Need help configuring VL53L8 firmware

Hello, I’m working on a project where I have a Nucleo F401RE connected to a 53L8A1 expansion board. I’m able to get the histogram plot with the ToF sensor on the expansion board but am wondering if I will still be able to get it if I use an external ...

ay0and0 by Associate II
  • 2011 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L4CX using VL53L4CD ULD

Hi!I've been testing the VL53L4CX sensor with its own API. I want to know if I can use the VL53L4CD ULD on my L4CX sensor and achieve the same performance as if I were using a L4CD ULD on the L4CD sensor. I've read similar questions on this forum reg...

LDMigotto by Associate II
  • 1226 Views
  • 1 replies
  • 2 kudos