User Activity

Hi, when using the VL53L1X, it is suggested to check for the range status and 0(zero) is considered the desired range status. Now, as I understand it, the range status 2(two) is dependent on the signal threshold. By default, the signal threshold is s...
Hi,Is there a way to obtain the actual SDAD location that is currently being detected. The reason for this is because I want to map out the locations and can see what are actually being triggered.I am using 4x4 ROI with 199 as the center.Thanks.