Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Advice on VL53L7CX and very high reflective fabric

Hello everyone,We recently tested the VL53L7CX and ran across an issue with very high reflective fabrics. Here are two images of such fabric. The first is a picture taken with flash light off, second picture is taken with flash light on. From the mom...

S1M_0-1745193280050.png S1M_1-1745193318610.png
S1M by Associate II
  • 2057 Views
  • 4 replies
  • 0 kudos

Resolved! register adresses

Hi, i am trying to connect the nrf54L15 with the VL53L4CD sensor. I am having trouble with library and the code. Struggling with connecting the nrf54L15 to the sensor in the different libraries. Are you able to share the different register adresses f...

espen by Associate
  • 631 Views
  • 1 replies
  • 0 kudos

Does anyone know of a module using the VD55H1?

I know the VD55H1 is in preview phase and might be difficult to get it from ST. Although from the you tube videos it seems it is ready to be requested. Do you know what is the status to get one sensor? And if maybe is there any design house offering ...

WDela.1 by Associate II
  • 4967 Views
  • 9 replies
  • 1 kudos

Resolved! Clarification in P-NULCLEO-53L8A1A

Hi Team,We have the two boards as mentioned below.                      The Code generated in Cube MX is for the F401RETX(which configures the MCU inside VL53L8CX)In the above diagram , the host is the F401RETX . Please confirm , if our understanding...

Image(8)(1).jpeg TOF.png
Vbala.1 by Associate II
  • 980 Views
  • 1 replies
  • 0 kudos

Resolved! Unreasonable Data from VL53L8CX Sensor

Hello Everyone, I am currently using the vl53lmz_uld_api  tto process data measured by the VL53L8CX sensor. I have also used the "example_12_cnh_data" to retrieve data from my sensor. However, the incoming data seems completely incorrect, and I don't...

kgb by Associate III
  • 5251 Views
  • 15 replies
  • 1 kudos

Resolved! Getting data from VL53L8CX using vl53l8cx_api

Hello  everyone,  I started learning programming on the STM32 ecosystem a few weeks ago, and I'm currently trying to get data from the VL53L8CX sensor using the NUCLEO-F401RE expansion boards and the vl53l8cx_api. I wrote a small program based on wha...

kgb by Associate III
  • 1260 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L8CX: Histograms manipulation and Interpretation.

Hello Everyone,I am currently working on a project to determine if it is possible to differentiate between a glass cup and other types of cups using VL53L8CX sensor data histograms, and also to detect the fill level. I have already collected data fro...

kgb by Associate III
  • 1904 Views
  • 4 replies
  • 0 kudos

Resolved! vl53l1x sensor initialization problem

I'm using the VL53L1X in the Arduino environment. During the initialization phase, I can read the device address as 0x29, and the device ID is EACC — so there's no issue with that.However, when I try to read the register VL53L1_FIRMWARE__SYSTEM_STATU...

eneeen by Associate II
  • 1340 Views
  • 1 replies
  • 0 kudos