Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Choice of ToF VL53

Hi All, I've been using the VL53L1 sensor for drone height control, and the results have been quite good- however, the environment it is used in has plastic skylights with poor IR blocking. This causes unstable readings in direct sunlight. Some of th...

DM575 by Associate
  • 595 Views
  • 1 replies
  • 0 kudos

VD6283TX45/1

Hello, I am using the VD6283TX45/1 to develop a device and now have a question to consult. Due to my insufficiently careful reading of the data sheet during the initial design phase, I connected the I2C pins of this device to an I2C bus where the pul...

FHL by Associate
  • 443 Views
  • 0 replies
  • 0 kudos

VL53L4CD emitted optical power value

Has anyone seen documentation or done optical power measurements for VL53L4CD? I’m trying to find the radiant energy or optical power output of this low power time-of-flight device. (I only succeed to find a graph showing the relative emitted power i...

VL53L4CD_Relative Emmited Power.png
ali_Kiwi by Associate
  • 568 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L0x Offset calibration and Crosstalk calibration

Hi    follow  can  make offset calibration?Place the object 14cm away .Must be in a dark environment?     follow can make Crosstalk calibration?   Place the object 60cm away. my coverglass like follow,The measured distance seems very short. How can...

zhy_0-1761292891871.png zhy_1-1761293001860.png zhy_2-1761293212141.png zhy_3-1761293684788.png
zhy by Associate III
  • 1933 Views
  • 14 replies
  • 0 kudos

IIO-based Linux driver for VL53L7CH

 Hi, we would like to use the VL53L7CH on Linux 6.12.Standard kernel interfaces are required:IIO/hwmon subsystems and regmap — no proprietary ioctl/miscdevice interface.Is an IIO-based driver for the VL53L7CH already provided or planned for upstream/...

VL6180X IEC 60825-1 CB test certificate

Hello ST:       VL6180X has been discontinued, but our older equipment still uses it. We hope to obtain the IEC 60825-1 CB test certificate to prove its Class 1 rating. However, this certificate is not available on ST's official website, whereas it i...

vl53l4cd variation in readings

Hi, We have incorporated a vl53l4cd into our product. We wish to measure 0 to 100mm with a resolution of 1mm, and an update rate of at most 1 second.We have set the vl53l4cd 19mm back from front measurement face (so we need to actually measure 19 to ...

Resolved! vl53l0x in continue and Time mode

Hi,        vl53l0x in continue mode ,how to read data_status and in time mode how to set time and read data and data_status?               thanks

zhy by Associate III
  • 802 Views
  • 4 replies
  • 0 kudos