Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L0X mechanical sizing information

We are developing sensing device with using VL53L0X,  we will use optical lens on top of  VL53L0X  for special sensing purpose then in order to optimize lens design with effecive sensing, we would like to know dimension of both sensor and emitting ch...

Hide1 by Associate II
  • 1541 Views
  • 7 replies
  • 1 kudos

Using VL53l0x with DMA

I have an application that needs to use several VL53l0x ToF sensors. The measurements need to be fairly responsive to a slow moving object approaching the sensor; so something like taking readings at 10Hz would be reasonable.  Having tried a quick pr...

MikeB100 by Associate II
  • 494 Views
  • 1 replies
  • 0 kudos

VB1940 Pinout

Hi ST Support.I am currently working with a camera module using VB1940. I could not find a detailed pinout or pin definition in the official documentation. I would greatly appreciate it if someone could help me with that.Thank you very much for your ...

Atoskdke by Associate
  • 599 Views
  • 2 replies
  • 1 kudos

Confusion on the VL53L1-SATEL registers

Hello, I am currently trying to write code for the I2C communication with the VL53L1-SATEL board. I was trying to confirm that the I2C was working by reading some registers mentioned in the VL53L1 Datasheet, those being 0xC0, 0xC1, 0xC2, 0x51, and 0x...

Carson by Associate III
  • 595 Views
  • 4 replies
  • 2 kudos

Resolved! Source available for STSW-IMG041 Device Code ?

Hi,I would like to know if the STSW-IMG041 code that is flashed into the device is available somewhere. My goal would be to use the same code but on a custom board to verify that the sensor is working properly.Thank you! 

MikeReg by Associate II
  • 604 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO C09RC-B03 and X-Nucleo 53lxA1

Hello everyone, I would like to know if someone has ever tried to couple those two hardware components together?I am currently using the STM32C092RC board to build an FD-CAN network, and I would like to exchange some real data — or more explicitly, t...

kgb by Associate III
  • 428 Views
  • 1 replies
  • 0 kudos