Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L0x

 Hi, the rear background exceeds 2 meters, and there are no obstacles in front of the sensor. The measurement data is unstable, and the reading sometimes reaches 0 and sometimes reaches 115.      

zhy_0-1761185641250.png zhy_1-1761186162004.png
zhy by Associate III
  • 3589 Views
  • 2 replies
  • 0 kudos

Reading measurement on VL6180X

STMicroelectronics support,I am testing a VL6180X laser sensor device for use in autonomous robotics.I currently get good distance measurements using an Arduino sketch but can't use that platform in my final product.Instead I'm using a pic18f46k22 mi...

jerryD by Associate
  • 606 Views
  • 1 replies
  • 0 kudos

VL53L8CX RUNNING SPD

Hello, I have a problem when I try to run the SPD code under STM32cube IDE, I have this under the serial monitor which remains stuck like this: SPD ULD SW Kit version 1.0.0Module type = VL53L8CXModule ID : 0000000000000000_VL53L8CBV0GC/1$2FW Version ...

Freedy by Associate II
  • 881 Views
  • 1 replies
  • 0 kudos

Resolved! vd66gy with Raspberry Pi5: Failed to Queue Buffer

I am using a pcb4188_vd66g1 camera module with a Raspberry Pi 5.The system has been freshly set up with Raspberry Pi OS 64-bit, and I followed the official setup guide step by step.After completing the setup:The camera is detected correctly when runn...

05_rpicam-hello--list-cameras.png 06_rpicam-hello_error.png 07_v4l2-ctl--list-devices.png 08_i2cdetect.png
Erebos by Associate
  • 971 Views
  • 2 replies
  • 0 kudos

Voltage drop when measuring with VL53L0X

Hi everyone,I’m working with the VL53L0X sensor and I noticed that when it starts ranging, the supply voltage (of my board with the VL53L0X, the Vcc pin) drops from 3.389 V down to 2.544 V.In this setup, the VL53L0X is powered from the 3.3 V pin of a...

Self test for vl53l8cxv0gc/1

Hi,Currently, we are testing vl53l8cxv0gc/1 by placing an object in front and moving it and reading the values. Is there a way to test the functionality of vl53l8cxv0gc/1 in a production environment? Is there a self test mechanism for this sensor?Tha...

VL53L7CX Motion power

Hi, I'm trying the VL53L7CX sensor for a prototype and I'm trying the example codes provided within  this page https://www.st.com/en/embedded-software/stsw-img036.html I'm experimenting the Example_10_motion_indicator and I'm able to display the "mot...

LudovicB by Associate
  • 809 Views
  • 2 replies
  • 1 kudos

Error in VL53L1X datasheet

On page 9 of https://www.st.com/resource/en/datasheet/vl53l1x.pdf, it is written:"Ranging is continuous, with a programmable delay between two ranging operations (called anintermeasurement period)"This is wrong. It should be:"Ranging is continuous, w...

paul19 by Associate III
  • 605 Views
  • 3 replies
  • 0 kudos