GNSS positioning

Ask questions and find answers on Teseo GNSS positioning solutions. Discuss NMEA sentences, SBAS activation, and signal troubleshooting.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Teseo-Suite Pro license

Hi,I bought an EVB-LIV4F to evaluate LIV4F and I have sent two emails to st-teseo-suite-support@st.com to request activation code. Unfortunately, I haven't received any response. Is it possible to check whether ST has received my request?Thanks.

kolee by Associate II
  • 1609 Views
  • 3 replies
  • 2 kudos

Resolved! X-STM32MP-GNSS2 Antenna

Hi,The BOM and almost all pictures of X-STM32MP-GNSS2 include a Taoglas antenna.Could you verify if an antenna is actually included or not, if I order an X-STM32MP-GNSS2?

rvl by Associate II
  • 4005 Views
  • 7 replies
  • 13 kudos

STA8090F4GBTR defect analysis requirement!

你好!这种材料(STA8090F4GBTR)在我们项目的生产测试中存在低功耗问题,缺陷率约为0.8%,给我们的生产和维护带来了极大的不便。我们现在需要贵公司的协助来分析芯片体缺陷的原因。谢谢!

hebin987 by Associate
  • 1024 Views
  • 2 replies
  • 1 kudos

EVB-LIV4F USB linux driver

Hi,I would like to know if EVB-LIV4F has USB linux driver. I would like to connect EVB-LIV4F to a ubuntu computer.Thanks,Koon 

kolee by Associate II
  • 939 Views
  • 1 replies
  • 0 kudos

Resolved! LIV4F actual VBAT range

What is the actual backup input supply voltage range for Teseo LIV4F receivers? Datasheet says that it is 3-3.63V which is really high and doesn't make sense to add any Lithium battery as a backup supply because it will very quickly drop below 3V at ...

Vane by Associate II
  • 2090 Views
  • 4 replies
  • 1 kudos

Teseo Suite activation

Hi, I am trying out EVB-VIC3DA and would like to use Teseo suite with full function. I am sending activation request e-mails to st-teseo-suite-support@st.com using request forms generated from Teseo Suite, but haven't received any response yet. Could...

ryomatsu by Associate
  • 3293 Views
  • 4 replies
  • 1 kudos

LIV4 firmware update with GSV frame error ?

hi everybody,i have some issue with the last update of the firmware for the liv4 4.6.3 : FreeRTOS V10.4.3_ARM , BINIMG_4.6.3_ARM, SWCFG_8606532, GNSSLIB_00000000_ARMactually, i have configure the mode for GPS only constellation and RMC+ GSV frame onl...