GNSS positioning

Ask questions and find answers on Teseo GNSS positioning solutions. Discuss NMEA sentences, SBAS activation, and signal troubleshooting.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Teseo-LIV4 GNSS Firmware Update CRC Error

I'm attempting to update the firmware for the LIV4 GNSS module, and everything seems to goes well until the CRC step, where it hangs for a few seconds then reports a failure. The module is no longer publishing any data, but when using the 'recovery' ...

JCharette by Associate II
  • 1489 Views
  • 10 replies
  • 1 kudos

TESEO LIV3FL Hot Start

Hi Community,I have been approaching the GNSS theory and the TESEO Hardware for few weeks and many questions come into my mind regarding the Hot Start and the Cold Start.First things first, I am using a custom PCB on whom surface  the TESEO, LTE modu...

TESEO III EVB PPS LED

Hi everyone,I am using the TESEO LIV3-FL EVB. Suddenly the PPS green led stopped to work and the device was simply connected via UART/USB to my laptop. This happen while I was trying to set a log data recording.Now I am trying to restart the evaluati...

TESEO-LIV4F Trouble using $PSTMEPHEM

Hi all, We're having trouble getting the module to respond to the message "$PSTMEPHEM" We're attempting to upload ephemeris data but the module is ignoring the message, ie: the module is not responding with either "PSTMEPHEMOK" or '"PSTMEPHEMERROR" T...

JCharette by Associate II
  • 1551 Views
  • 7 replies
  • 4 kudos

Resolved! Teseo LIV4F NO FIX

Hi team, i have built a custom gnss application for my UAV, using the teseo liv 4f module.i have attached my circuit herewith, and also the corresponding output from the teseo suite.The module has no fix always and is not locking onto any sat.please ...

CKT.png TESEO.png

Teseo-LIV4F Diplexer/multiplexer

Hi all. I have a Teseo-LIV4F that I am working with. My project has an L1 and an L5 antenna as the receiving antennas.I am looking to feed a combination of L1 and L5 into the Teseo-LIV4F. I obviously need a diplexer/multiplexer of some sort so that I...

designing with STA8135

Hi.I want to use the STA8135 chip in my circuit board.the datasheet doesn't have any application notes, like power filtering requirements, individual pin description, method of GNSS data transfering etc.Is there an application note somewhere that I'm...

yobren by Associate
  • 468 Views
  • 1 replies
  • 0 kudos

synchronizing multiple GNSS receivers (Teseo v)

Hi.I want to use two GNSS receiver ICs from the Teseo v family (either STA8100 or STA8135).It is important in my application that the 3-bit ADC sampling of both receivers will be synchronized.The IC has a TCXO input which obviously is used as the ref...

yobren by Associate
  • 1229 Views
  • 0 replies
  • 0 kudos