| Subject | Author | Posted | |
|---|---|---|---|
|
I would like to know if it is possible to generate a sweep signal (a sine wave with increasing freq...
| 2024-07-04 11:31 PM | ||
|
I'm developing a vibration and temperature analysis system. To do this, I have developed a sensor ...
| 2024-07-04 6:40 AM | ||
|
Hi, While implementing a single conversion process for the Analog-to-Digital Converter (ADC) via ...
| 2024-07-02 10:09 PM | ||
|
I am making this code which, on an interrupt, is supposed to wake the system from STOP mode, put it...
| 2024-07-02 7:47 AM | ||
|
Hello, After reading the following threads: How to program STM32 Option Bytes with the HAL API - ...
| 2024-06-28 6:12 AM | ||
|
Hi there, I have some question about the deferent about the source code and the lib. For example,...
| 2024-06-27 8:13 PM | ||
|
I am using NUCLEO-G071RB. I use 2 ADC channels: GPIO analog and internal temperature sensor. I conn...
| 2024-06-27 6:00 AM | ||
|
Hello guys! I have a problem. I need to use HAL_RTCEx_SetSynchroShift function from HAL to modify t...
| 2024-06-26 11:10 AM | ||
|
I found a confusing phenomenon that I found when using STM32G431CBU6 OPAMP3 works in Timer controll...
| 2024-06-26 7:27 AM | ||
|
I am using STM32H5 nucleo board and it is connected with MIC which gives PDM output based on analog...
| 2024-06-26 4:36 AM | ||
|
Hello, I am doing a project on making a car display using STM32H735, but the Display on it is small...
| 2024-06-25 9:45 PM | ||
|
Hello ! I'm new here and I'm new to programming with a big project. I ordered a Nucléo F401RE wit...
| 2024-06-25 2:00 PM | ||
|
At present, when STM32L412 uses the HAL_SPI command to read back the Register, no matter which Regi...
| 2024-06-25 2:20 AM | ||
|
Hi ST tesam, When I use the HAL of STM32C031, I have some trouble about SMBus. Q1:When I use the ...
| 2024-06-24 1:18 AM | ||
|
I want to connect 2 Nucleo F103RB as slave (2 Nucleo slaves) to one master (PC for now) over Modbus...
| 2024-06-23 9:42 PM | ||
|
Hello, I've a project with the STM32G030F6 which the application use in 90% of time the low power ...
| 2024-06-21 1:09 AM | ||
|
I am working on an application using an STM32U5A5 nucleo board with four MEMs PDM output format mic...
| 2024-06-20 11:49 AM | ||
|
I am experiencing an issue with the Dual Boot Bank Swap Boot Loader on my STM32G474RE microcontroll...
| 2024-06-20 7:10 AM | ||
|
Hello,
I have a issue to control IS66WVE4M16EBLL-70BLI with STM32U585AII6.
Although IS66WVE4M16...
| 2024-06-20 1:39 AM | ||
|
The software drives the SPI to drive the RF chip, and I add a 0r resistor to the SPI as shown in Fi...
| 2024-06-19 5:10 AM |