Hi, I bought a Teseo-VIC3DA Evaluation Kit and when I went through the associated documents, they mentioned the concepts of "Teseo-DRAW and Teseo-DRUM". In my application, we do not have access to t...
Hello! Is external antenna included with X-NUCLEO-GNSS1A1 board (or X-NUCLEO-GNSS2A1) or it should be purchased separately? GNSS expansion board based on Teseo-LIV3F module for STM32 Nucle...
I installed the Teseo-VIC3DA Evaluation Kit to my car and drove for about half an hour. The "sr" field of PSTMDR2 showed "system ready". Then I disconnected the antenna to test the DR mode. The ...
Hi, Due to the limitation of height in our product, modules won't be suitable. I am currently considering STA8089FG. Could you send me the application note/reference design for this chip? Thanks.
Hello! Can you please help with the differences between Teseo-LIV3FL and Teseo-LIV3F modules, does LIV3FL have all the features of LIV3F plus low power, are there any reasons why to prefer...
I have recently procured a X-NUCLEO-GNSS1A1 on its own. I would simply like to use the LIV3F to test the LNA/SAW filtering along with different antennas as well. I am able to connect the LIV3F t...
Hi Team, In this module(TESEO-LIV4f) can able to processing the data L5 band(NACIC data and IRNSS) And how to update the firmware for l5 band(navic and Irns...
Hi all, I have been doing some experimentation with a LIV4F module and am trying to configure the device for a 5Hz data output rate. I see the device supports up to 10Hz. The commands I have tried ...
What is the actual backup input supply voltage range for Teseo LIV4F receivers? Datasheet says that it is 3-3.63V which is really high and doesn't make sense to add any Lithium battery as a backup su...
Hello, In document UM3009 §7.3 => Multi-constellation firmware supports the following constellations: GPS, GALILEO, GLONASS, BEIDOU and QZSS. All constellations cannot be enabled at the s...