...icense text: vvvvvvvvvvvvvvvvvvvvvvvvvvvv beginline=9 vvvvvvvvvvvvvvvvvvvvvvvvvvvvv # This file is free software; you can redistribute it and/or modify it # under the terms of the GNU General Public L...
I could not download the STM32MP starter package. The login and download page simply cycle and the download does not happen. Wondering if anyone else encountered this issue.
I'm using the Board STM32MP157F-DK2 on a Linux Ubuntu 22.04 I was trying to follow the 1.3.1 step at 'https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_Starter_package#Install_all_X-LINUX-AI_package...
Hi, I've been following along with the "Getting started" on the wiki, but I cannot set up the developer package for my STM32MP157x-DK2. Downloading the file and trying to extract the archives, I get...
optee-stm32mp-addons repository is not available in github. Seems to be deleted or cant be accesed. URL: https://github.com/STMicroelectronics/optee-stm32mp-addons
Using MP135F-DK board. Setup the environment and rebuild kernel. After I use openocd and gdb success connect to linux system, try to debug linux kernel, then run some simple gdb command like "bt" o...
Custom board based on stm32mp151a. Migrating from kirkstone to mickledore and from SP_MIN to OPTEE. usart1 assigned for debuging, uart4 and uart7 for modbus communication. I cannot boot uboot with u...
Custom MP157AAA3 board. SD card formatted with ECO 5.0.0 using the SD tools using the files from the starter package. (including rootfs etc..) . Build the TF-A, OP-TEE (in SYSRAM), U-boot...
Run bitbake rep and sync and DISTRO, then bitbake , it shows the EULA and the build start, interrupt the build by press CTRL-C, closing the console window and re-entering it. then start bitbake, belo...