Hello I have an STM32MP135x-DK board and have built my own openstllinux image and rootfs for it as shown in this article. https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package Now I...
I have made my own STM32MP1 board with the STM32MP151AAC3 processor. Right now I'm faceing issues with the software STM32CubeProgrammer and I don't know why this happens. My goal is to flash the eMM...
Hi,all I noticed that the ethernet driver stm32mp13xx_hal_eth.c in the STM32CubeMP13_V1.1.0 already supports PTP, When will STM32CubeMP2 package be available, and since the STM...
Hello everyone, I am trying to debug a custom board with STM32MP151 with WM8988 connected with SAI2, the connection is just as STM32MP15x-DK with except that there is no I2S to HDMI. The...
@Erwan SZYMANSKI Hello, I am having trouble with another topic . I was learning how to modify my distribution packet . I started with learning how to change backlight of my daughter board (ım using ...
Hi there, During OP-TEE integration of our custom platform based on STM32MP151C MPU I'm facing an issue with DFU. It looks like the dfu command stucks in `run_usb_dnl_gadget` inside the loop a...
I have STM32MP157A-DK1 board I am using distribution package. I want to add c++ library based on cmake to my distribution. I crated the recipe using command devtool add --no-same-dir ../pass/to/m...
Im attempting to set up A/B partitioning on an STM32MP157d-dk1 board so that it can switch between partitions when updating. The board image is built using yocto, and I have used the meta-st-stm32mp ...
Hi,
I'm discovering the STM32MP13 Bare metal project. I'm following example given by the STM32CubeMP13 Package.
Everything works fine except for the fact that I'm disappointed by the per...
https://community.st.com/s/question/0D53W00000PoivmSAB/changing-the-emmc-pins-with-otp I have the same pin mapping as above: SDMMC2_CK - PE3 (AF09) SDMMC2_D0 - PE6 (AF07) SDMMC2_CMD ...