2023-10-23 07:10 AM
Dyslexic reference to SMT32
https://www.st.com/en/microcontrollers-microprocessors/stm32f469-479.html
"The STM32F469 and STM32F479 lines deliver the highest Arm® Cortex®-M4 performance and embed large memories and rich peripherals to enable the most advanced consumer, industrial and medical applications. The ART Accelerator™ for Flash memory and the Chrom-ART Accelerator™ for graphics coupled with LCD-TFT and MIPI-DSI display interfaces enables an advanced user interface while granting enough resources for demanding real-time processing.
The STM32F469 and SMT32F479 product lines provide from 512 Kbytes to 2 Mbytes of Flash, 384 Kbytes of SRAM and from 168 to 216 pins in packages as small as 4.89 x 5.69 mm."
Solved! Go to Solution.
2023-10-23 08:08 AM
Thanks @Tesla DeLorean . I will pass it to the respective team.
2023-10-23 08:08 AM
Thanks @Tesla DeLorean . I will pass it to the respective team.
2023-10-23 08:50 AM
It's a relatively widespread typo, I guess there are more instances of it throughout "main" st.com (and of course much more on community.st.com). Webmaster might search for "SMT32*" in the web's textual sources.
JW
2023-10-23 02:29 PM
I do see this a lot on this forum, and others. Sometimes even more mangled.
Just was surprised to catch it on an ST page.
2023-10-24 02:21 AM
Thanks @waclawek.jan , good catch! I will pass it to the respective team to check.