cancel
Showing results for 
Search instead for 
Did you mean: 

Please support .zip attachments

The forum allows .z, .7z, but does not allow .zip attachments.

Please fix.

JW

1 ACCEPTED SOLUTION

Accepted Solutions
Laurids_PETERSEN
Community manager
Community manager

Hello @waclawek.jan and all,

I'm happy to let you know that .zip files are now allowed in the community.

Best regards,
Laurids  

 

View solution in original post

14 REPLIES 14
RhSilicon
Lead

:see_no_evil_monkey:

+1

Not any more intrinsically safe / unsafe as an other archiving method, and can be scanned. Lack of support just adds to reasons not to participate.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Lina_DABASINSKAITE
Community manager
Community manager

Hello all, 

The type: .zip is excluded due security recommendations. Let me please check internally what could be done about it. 

BR,
Lina

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Johi
Senior III

Very good proposal. On top of this the 5 MB limit is also a bit outdated. At least we should be able to share zipped example programs to support each other and indirectly ST.

The security issue would be WHAT'S IN THE ZIP, the integrity of the files can be readily established, and the content scanned for threats.

Don't allow them to contain EXE/DLL files, or be password protected / encrypted.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Piranha
Chief II

Tried adding some files to this topic:

https://community.st.com/t5/stm32-mcus-embedded-software/how-to-make-ethernet-and-lwip-working-on-stm32/td-p/261456

Piranha_0-1701025175036.png

The RAR, 7Z, TAR and XZ archives are supported, but not ZIP because of "security". Also does any of those "security experts" even know that a DOCX, XLSX and PTPX files are also ZIP files with a different extension? @Lina_DABASINSKAITE , do you have any clue what level of nonsense you are talking here?

Oh, but it lists HEX as an accepted format - let's try that...

Piranha_1-1701025545502.png

A perfectly normal HEX files "does not match its file extension". One can see those HEX files added to that topic as a TXT files.

This is still a bug. As explained above, "security concern" is nonsense.

JW

.docx are ZIP files..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Lina_DABASINSKAITE, @Amelie ACKERMANN , can this please be rectified asap.

We need to be able to exchange packs of files. .zip is an industry standard, and, as pointed out by many, other packed formats (some of which are proprietary thus require installing/running proprietary unpackers, hence pose a significantly larger security risk) are allowed; and also formats which in fact have the same underlying .zip structure.

In other words, the quoted security concerns are moot.

We need to exchange .hex and .elf files, too - either standalone or as part of .zip  - those result from source files compilation and are vital for being able to help users with specific problems which stem from the compilation process. Those don't pose any significant security issues either, as they are not run on PCs but on microcontrollers.

JW