Help deleting my account
Hello,Can the admin please help deleting my account permanently?If you are admin and read this then please do so asap. @admin
This forum is to raise questions or provide feedback only linked to the community platform.
Hello,Can the admin please help deleting my account permanently?If you are admin and read this then please do so asap. @admin
Doesn't happen in the thread itself: https://community.st.com/t5/stm32-mcus-embedded-software/stm32l4-hal-rtc-functions-do-not-check-hrtc-gt-instance-before/m-p/703427
The forum allows .z, .7z, but does not allow .zip attachments.Please fix.JW
This notification is incorrect. This user created a new topic and did not reply in this topic: This notification is also incorrect:Two unrelated notifications got merged. I saw this happen once before and I was confused about it.I use Firefox.
I kept coming back to this website to download the STM32 Cube IDE and the servers would always be down once I tried to log in and download it.I've noticed some forums from 2019 mentioning similar problems with how slow the website is responding, so i...
If A asks a question and B replies. If B subsequently returns to edit her reply the prompt she gets above the edit box is "Edit your reply to B". Which is wrong, it should be "Edit your reply to A". More simply, why not just have it say "Edit your re...
See for example this helpful post by @Andrew Neilhttps://community.st.com/t5/stm32-mcus-products/stm32-ic-s-unique-id/m-p/657372/highlight/true#M239912 Andrew is a stand-up guy. He wouldn't be this sloppy when posting, but it's not his fault.Whenever...
When you subscribe to a thread with multiple participants and a single participant adds a reply, you get a notification.But the title of the notification includes the name of everyone in the thread who have commented so far ("A and B replied to topic...
For example here:https://community.st.com/t5/stm32-mcus-products/timer-compare-output-using-dma-stm32f3discovery/td-p/672897there are two code blocks with "View more",buttons. When "View more" on the first code block is clicked, both code blocks are ...
Also broken in the '@' lookups:Except, perhaps, Ascha.3: