2024-11-21 05:53 AM
Hello,
I would like to know how to send a ZIP file in a private message. I don't have this option at the bottom of the page
But I have only theses option at the Top of the page :
And with this options, I can't send anything.
Thank you
Solved! Go to Solution.
2024-11-21 07:40 AM - edited 2024-11-21 07:43 AM
2024-11-21 06:24 AM
@DYann.1 wrote:I don't have this option at the bottom of the page
Hmmm ... It's there for me:
As it's a private message, you could just agree with the other party/ies how you want to exchange files - maybe via a 3rd-party site or service ...
2024-11-21 06:30 AM - edited 2024-11-21 06:31 AM
In the private message I said not in the standard message :
I have nothing. Yes via a 3rd-party site or service is possible but the correspondent does not accept much. So Why we don't have the possiblity to send a ZIP file in the private message ?
2024-11-21 06:30 AM
Hello,
And the size of the file should not exceed 250MB.
@DYann.1 what is is the size of the file you need to share?
2024-11-21 06:36 AM
yes, that is a Private Message!
2024-11-21 06:39 AM
Even in private message you can share files:
2024-11-21 06:40 AM - edited 2024-11-21 06:48 AM
The size is 1,05 Mo. Another way, could you contact me via my professional email ? Is it possible for you ?
2024-11-21 06:45 AM
I don't have this picture as you have. I only have this picture (in the private message I say)
2024-11-21 06:53 AM
My earlier post was creating a new PM.
even replying to an old PM, I do have the 'Drag and drop files to attach' box:
Looks like some setting or restriction on your account?
2024-11-21 07:01 AM
Hi @DYann.1 and @Andrew Neil,
The reason why @DYann.1 can’t send a private message, is because the permission to attach local files isn't granted at this time.
Some permissions are based on our community rank system. We’ve noticed a misuse of the private message functionality from spammers, which is why we’re testing changes to private messages and private message attachments.
We want to find the right balance between preventing spam, and not disrupting private messages for active community users.
We’re actively working on it, it's still in progress, and you can expect additional changes very soon.
Best regards,
Laurids