2023-05-23 06:55 AM
screen MB1166-a09,FP-AI-VISION1_V3.1.0,camera mb1683-CAMS-A02, the screen is a mess.No camera picture.
I'm using cubeide for run( flash the borad),should i change the version of FP-AI-VISION1? where i goes wrong?
Solved! Go to Solution.
2023-06-02 06:00 AM
Hello @wjian.2 ,
The fix is available on GitHub :
In fact , LCD DSI MB1166-A9 delivered with latest version of STM32H747I-DISCO/ boards come based on LCD FGRIDA FRD400B25025-A-CTK instead of FRD397B25009-D-CTK.
Now the firmware is updated , you just need to enable the right hardware component as defined in stm32h747i_discovery_conf.h file and add the new component library (NT35510) in your project .
/* IMPORTANT: One of the following flags must be enabled in stm32h747i_discovery_conf.h file */
/* options in order to select the target daughter board revision connected on STM32H747I DISCOVERY : !!!!!!!!!! */
/* USE_LCD_CTRL_OTM8009A */ /* Applicable for all LCD daughter boards (MB1166) except for Rev -A09 */
/* USE_LCD_CTRL_NT35510 */ /* Applicable only for LCD daughter boards (MB1166) Rev -A09 */
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-23 08:49 AM
Hello @wjian.2 ,
First of all let me thank you for posting your issue.
Which STM32H747I-DISCO revision are you using? MB1248-H747I-D02, MB1248-H747I-D03 ...?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-23 09:15 AM
DK32H747I$AT2,the turn to use FP-AI-VISION1 is copy the file binary to the board then compiler project in cubeide no?
2023-05-24 02:05 AM
Hi @wjian.2,
I confirm the issue and I reported internally.
Internal ticket number: 152907 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-06-02 06:00 AM
Hello @wjian.2 ,
The fix is available on GitHub :
In fact , LCD DSI MB1166-A9 delivered with latest version of STM32H747I-DISCO/ boards come based on LCD FGRIDA FRD400B25025-A-CTK instead of FRD397B25009-D-CTK.
Now the firmware is updated , you just need to enable the right hardware component as defined in stm32h747i_discovery_conf.h file and add the new component library (NT35510) in your project .
/* IMPORTANT: One of the following flags must be enabled in stm32h747i_discovery_conf.h file */
/* options in order to select the target daughter board revision connected on STM32H747I DISCOVERY : !!!!!!!!!! */
/* USE_LCD_CTRL_OTM8009A */ /* Applicable for all LCD daughter boards (MB1166) except for Rev -A09 */
/* USE_LCD_CTRL_NT35510 */ /* Applicable only for LCD daughter boards (MB1166) Rev -A09 */
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.