Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! there is some problem in SPI config based on SPC58NN

hello guys, I want to config SPI to communicate with TJA1145 .the 4 pins are shown in the picture. but I test the signal by OScilloscope and I found nothing in the four pin which means no meaningful signal. for example the CS pin is always high and n...

0693W000005CC3uQAG.png 0693W000005CC3zQAG.png
Yqiu.1 by Associate II
  • 1487 Views
  • 1 replies
  • 0 kudos

Resolved! Which paths should I include to correctly compile the "SPC58ECxx_RLA Network Ping Test Application for Discovery" example

I have the following configuration, but although I include the ones that I consider correct, I still get many errorsThe errors are supposed to be related to the tcp-ip component, but I already included it and I don't understand what is wrong, maybe I...

0693W00000Nq7VqQAJ.png 0693W00000Nq7VaQAJ.png
by Not applicable
  • 1560 Views
  • 4 replies
  • 1 kudos

Resolved! I configured 86 slot one cycle , but configurable message buffer number of the first message buffer segment and second buffer segment are total 32 . So do i read/write all slots in cycle despite message buffer number is 32?

I am currently developing a Flexray driver. I cant understand a few point. This message buffer configurable like that : "configure each message buffer by setting the configuration values in the Section 21.5.2.65: Message Buffer Configuration, Contro...

AYazı.3 by Associate II
  • 4792 Views
  • 6 replies
  • 0 kudos

Resolved! SPC5 studio PPCFREEGCC with VLE support version 4.9.2 Plugins.

Hello everyone,I'm struggling trying to compile an old project without having to regenerate the configuration files, this project was made under the ppc freegcc with vle support V4.9.2 ,I tried to compile using the last actual version(4.9.4) and I'm...

CBena.2 by Associate
  • 1969 Views
  • 1 replies
  • 0 kudos