Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

iSYSTEM winIDEA plugin for Eclipse

Posted on August 14, 2014 at 12:51Hello, I am using the iC5000 from iSYSTEM for programming and debugging. ISYSTEM provides a winIDEA plugin for Eclipse. Does anybody know if this plugin is supported by SPC5 Studio? Or has anyone even tested the plu...

Patriks by Senior
  • 821 Views
  • 1 replies
  • 0 kudos

Resolved! Problem with external interrupt

Posted on July 27, 2014 at 10:01Hello, This question is propably really basic, but I hope to get any advice, a link to a tutorial or even a sample code which helps me to solve my problem. I am really new in this buisness. The possibilities of the SP...

Patriks by Senior
  • 2313 Views
  • 5 replies
  • 0 kudos

Resolved! External RAM SPC564A example project?

Posted on August 04, 2014 at 17:22Are there any example projects for the SPC564A on the SPC56xxMB EVAL board that show how to use external RAM?If not complete projects, any code snippets or even hints or advice?ThanksKevin

Resolved! Flaxray Driver

Posted on July 31, 2014 at 10:13Hello, Are any FlexRay available for SPC56 devices? Thanks 

anton by Associate
  • 1104 Views
  • 2 replies
  • 0 kudos

how to flash binary into spc563M-disp board?

Posted on July 30, 2014 at 04:54I've compiled some code & I have .bin/.dmp/.elf/.hex/.map files. How do I program/flash whichever I need to flash into spc563M-disp board? I do have a PLS device, the driver and UDE Desktop installed. While AN4425 pro...

arro239 by Senior
  • 886 Views
  • 1 replies
  • 0 kudos

Cannot run program ''make''

Posted on July 24, 2014 at 12:44Hello, I installed SPC5 Studio and everything works fine and then after a view hours of working, i can´t build my project any more. I am always getting following error and i don´t know why: make -j4 all Cannot run pr...

Patriks by Senior
  • 1461 Views
  • 3 replies
  • 0 kudos

Resolved! IO Function Switching

Posted on July 15, 2014 at 21:38I have a project that requires an IO pin to switch between High Z (Tri-State) and High. On a previous 8 bit micro the high z condition was satisfied by setting the port to an input and the high was satisfied by making...

dwarnke by Associate II
  • 1408 Views
  • 1 replies
  • 0 kudos

update software ''Read timed out''

Posted on July 15, 2014 at 16:05Hello, The software update complains (see below log). The proxy is correctly configured. The update list is found but when it downloads the files, the error is coming. My browser can access the jar file so the links a...

make: *** [build/obj/boot.o] Error 2

Posted on July 07, 2014 at 17:51Hi, I hope this error is common for Eclipse users... Directly after installing SPC5 Studio V3 and setting up the one-year licence, I'm able to get all SPC56EL60L5 examples from the SPC5 Studio Wizard working (on the b...