Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC560P40 CAN driver development

I need help to develop SPC560P40 CAN driver as the examples given for that is complex and difficult to understand .Is any other document or examples code available, which is simple or uses register level programming?

How to disable JTAG?

Is it possible to disable JTAG completely on a SPC564B MCU using software?Reading the documentation about the censorship feature, it only seems to disable access to flash. Is it still possible to access SRAM and registers via JTAG when censorship is ...

SPC570Sxx Programming on Linux

Hello everyone,   Is it possible to program the SPC570Sxx series microcontrollers (specifically, SPC570S40E1) in Linux? I have been using PLS UDE-STK for programming under Windows but as far as I know there is no Linux version of that. Debugging capa...

Resolved! Asynchronous SPI Slave Mode on SPC572L64E3

Has anyone had any luck setting up the SPC572L64E3 to run in Asynchronous SPI Slave Mode? I need interrupts to trigger for chip select assert/deassert, tx word push and rx word pull. I've tried using the TFFF and RFDF ISRs but it seems that the TFFF ...

JLand.16 by Associate
  • 1661 Views
  • 2 replies
  • 0 kudos

Serial number for SPC5-CONEXPLORER

Bought SPC5-CONNECT but CD-ROM did not come with.So I ask,1. Is serial number for SPC5-CONEXPLORER in the CD-ROM which comes with SPC5-CONNECT?2. What are in the CD-ROM?Can anybody help me out?

TLee.16 by Associate II
  • 919 Views
  • 0 replies
  • 0 kudos

Resolved! Questions about SPC5 Studio Install and eco system for SPC58 devices

Dear all,I just ordered the SPC58EC-DISP eval kit and thought it's time to start to setup my first program. I downloaded and installed the SPC5 studio and run immediately into the following problems:When I try to install the GNU CC compiler from the ...

mkrug by Associate III
  • 3083 Views
  • 3 replies
  • 0 kudos

Resolved! Unable to connect to SPC58EC-DISP board through UDE debugger.

I am trying to connect to the SPC58EC-DISP board through PLS UDE Starter kit to program and debug the Serial Test Application example provided with the SPC5 Studio IDE. After opening the debug.wsx in the example project file on PLS UDE, an error appe...

AChie by Associate
  • 2391 Views
  • 1 replies
  • 0 kudos