2024-05-19 11:34 PM
Hi community,
I have implemented AVAS, I am getting the output as expected but with one issue that even after I stop communication in the CANoe , I am getting the sound continuously.
I wanted to know two things
1. Do we have any API that stops the sound just after stopping the communication in CANoe?
2. I thought of using the timeout functions that gets called after some time after stopping the communication so for this I wanted to know do we have any API or do we have any configuration settings?
Thanks,
Aishwarya UM
2024-05-19 11:58 PM
Hi,
No there is no CAN message to start/stop the sound.
See answer to similar question in the above post.
Best Regards,
AutoDevKit Team
2024-05-20 1:17 AM
Hi Max Vizzini,
I think you took the question in the other way. I am not asking about the CAN message that we need for start/stop sound. actually I have used entirely different messages and signals for my coded. I am not using the existing messages that are available in the base source code.
My doubt is,
1. I wanted to know do we have any API that particularly meant for activating and deactivating the Sound as like the hardware button(I mean I want a API which works as hardware button).
2. If there is no any such API,s then I am planning to use timeout function so I wanted to know is there any timeout API's or do I need to modify the configurations so that timeout API's gets enabled if any.
Thanks,
Aishwarya UM
2024-05-20 1:54 AM
Hi,
>>1. I wanted to know do we have any API that particularly meant for activating and deactivating the Sound as like the >>hardware button(I mean I want a API which works as hardware button).
No, there is no API.
>>2. If there is no any such API,s then I am planning to use timeout function so I wanted to know is there any timeout >>API's or do I need to modify the configurations so that timeout API's gets enabled if any.
No, there is not such an API.
Best Regards,
AutoDevKit Team