cancel
Showing results for 
Search instead for 
Did you mean: 

want to know the CAN BUSOFF is implemented or not In "Avas Compact - Test Application".

shiva_shankar_e
Associate III

hi community,

                      I am using the "Avas Compact - Test Application" example code which is provided in the AUTODEVKIT. hear I enabled the CAN communication and it is working fine. but i want to know CAN BUSOFF is implemented or not in the given example code. if not how to implement the CAN BUSOFF.

regards

shiva

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

>>    i just want to know the "CAN BUSOFF" is implemented or not.

No, not implemented.

Best Regards,

AutoDevKit Team

View solution in original post

3 REPLIES 3
Max VIZZINI
ST Employee

hi,

In the original code, the CAN messages are used to increase/decrease volume and engine speed and not to start/stop the sound.

There is a button on the board to start the engine. You should implement a similar code to start the engine with a CAN message.

Best Regards,

AutoDevKit Team

hi 

    i just want to know the "CAN BUSOFF" is implemented or not.

Hi,

>>    i just want to know the "CAN BUSOFF" is implemented or not.

No, not implemented.

Best Regards,

AutoDevKit Team