AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Set JTAG password lock SPC58EC80E5/AEK-MCU-C4MLIT1

Hello, I'm working with the AEK-MCU-C4MLIT1 board, which features the SPC58EC80E5 MCU. While using UDE STK 5.2, I noticed that the JTAG connection is always successful, regardless of the password set to unlock it. This suggests that the JTAG password...

Johxp by Associate
  • 1769 Views
  • 1 replies
  • 0 kudos

Resolved! AEK-POW-BMS69EN Custom Battery Project

Hello, I plan to make a 333V Battery using AEK-MCU-C4MLIT1 as the master, AEKSCOM-ISOSPIA as the translator and AEK-POW-BMS69EN as the slave BMS Boards.  So far, I have been using the Example "SPC58EC—AEK_POW_BMS63EN_SOC_Estimation_Single application...

Vipuls by Associate III
  • 2250 Views
  • 1 replies
  • 0 kudos

Resolved! AEK-POW-BMS63EN Short CIrcuit on Daisy Chain

Hello Community, I have an observation from my attempt to daisy chain multiple AEK-POW-BMS63EN devices.  I have made a battery pack which has two 14-cell Battery modules in series. One module is supposed to be connected to one AEK-POW-BMS63EN and sen...

Vipuls by Associate III
  • 3572 Views
  • 4 replies
  • 2 kudos

Resolved! BMS Chain Setup Assistance

I posted recently about getting set up with the demo for the GUI application, and got great help from @SRomeo. I've now moved on to the SingleAccess Chain demo, and could use some more help if you don't mind?I am using the C4ML1T, ISOSPI1, and 2 BMS6...

ISO_MCU Pinouts.png
Luke_A by Associate II
  • 3458 Views
  • 7 replies
  • 2 kudos

Resolved! AEK-MCU-C4MLIT1 BMS with CAN Project

Hello Community,I am trying to build a 333V Battery Pack with AEK-MCU-C4MLIT1 as the Master, AEK-ISOSPI Translator and multiple AEK-POW-BMS69EN as slaves in daisy chain configuration. I would like to get the information such as cell voltages, SOC, an...

Vipuls by Associate III
  • 5568 Views
  • 4 replies
  • 1 kudos

Resolved! AEK-POW-BMS63EN showing incorrect cell voltages

Hey, I am trying to build a battery pack with AEK-POW-BMS63EN BMS Slave Boards, AEK-MCU-C4MLIT1 as the Master Board, and an ISOSPI Translator.  I have made a 4S Dummy Battery to check whether I could get the cell data on the serial bus from the Maste...

Vipuls by Associate III
  • 2128 Views
  • 2 replies
  • 2 kudos