2024-11-28 5:39 AM - last edited on 2024-11-28 5:43 AM by Andrew Neil
Dear community,
I am exploring the use of AutoDevKit for the battery management of my battery in my project. I watched all videos and read through the manual for the AEK-POW-BMS63EN. However, I am new to this environment and need some help with the following procedure.
Thank you very much for your help.
Camillo
2024-11-28 5:43 AM
Hi,
Yes, the best is to start using our HW and SW and import an existing project(s) from AutoDevKit.
Because the source code is all visible, you can first run it and then put it in debug mode by setting breakpoints to understand the internal logic.
Only after these steps are completed, you can start defining a new BMS application by creating a new AutoDevKit project and adding the BMS Chain components.
Best Regards,
AutoDevKit Team
2024-11-28 5:55 AM
Hello Mr. Vizzini,
thank you very much for your help. Is the SPC58EC – AEK_POW_BMS63EN_SOC_Estimation_Single application for discovery demo a good starting point? Or do you suggest another demo?
Best regards,
Camillo
2024-11-28 5:59 AM
Hi,
Please use the new driver version 'CHAIN'
Best Regards,
AutoDevKit Team
2024-11-28 6:03 AM
Hello Mr. Vizzini,
my board is the BMS63EN and not the BMSWTX. Is there a different procedure or does it work the same?
Kind regards,
Camillo
2024-11-28 7:53 AM
Hi,
AEK-POW-BMS63EN + AEK-COM-ISOSPI1 is equivalent to AEK-POW-BMSWTX.
From HW point of view, either you use the 2 boards, or you use a single board.
Both configurations need to be connected with MCU (AEK-MCU-C4MLIT1).
If you need a battery holder, you can use AEK-POW-BMSHOLD (14 cells in series, one full BMS node).
Best Regards,
AutoDevKit Team
2024-11-29 7:17 AM
Dear Mr. Vizzini,
thank you very much for your help.
As I review the software, I’m unsure whether it’s necessary for me to understand every line of code in order to successfully test the BMS on some cells. Given this, I’m wondering if just flashing the demo code onto the board would be sufficient for these tests.
If you think another approach would be more effective, I’d appreciate your advice. While I have some theoretical knowledge of BMS functionality and its importance, I have limited experience with coding or selecting the appropriate APIs.
Thank you very much again
Camillo
2024-11-29 7:21 AM
Hi,
Approach it in an onion-skin fashion. Start to understand the general behavior first and dig inside step-by-step when needed.
Best Regards,
AutoDevKit Team
2024-11-29 7:59 AM
Good evening,
thank you very much for your answer. Do you also provide a GUI for keeping track of the battery parameters ?
best regards
Camillo
2024-11-30 4:34 AM
Hi,
Yes, there is a GUI you can find in the older driver examples (does examples not containing the keyword 'CHAIN') inside AutoDevKit. Next year we will release a GUI also for the CHAIN examples.
Best Regards,
AutoDevKit Team
P.S. Refer to below post
New beta release of BMS GUI for AutoDevKit solutio... - STMicroelectronics Community