AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! AEK-MCU-C4MLIT1 BMS with CAN Project

Hello Community,I am trying to build a 333V Battery Pack with AEK-MCU-C4MLIT1 as the Master, AEK-ISOSPI Translator and multiple AEK-POW-BMS69EN as slaves in daisy chain configuration. I would like to get the information such as cell voltages, SOC, an...

Vipuls by Associate III
  • 5735 Views
  • 4 replies
  • 1 kudos

Resolved! AEK-POW-BMS63EN showing incorrect cell voltages

Hey, I am trying to build a battery pack with AEK-POW-BMS63EN BMS Slave Boards, AEK-MCU-C4MLIT1 as the Master Board, and an ISOSPI Translator.  I have made a 4S Dummy Battery to check whether I could get the cell data on the serial bus from the Maste...

Vipuls by Associate III
  • 2188 Views
  • 2 replies
  • 2 kudos

Resolved! BMS63EN 14 Cell GUI

Hello,I am trying to set up the 14 cell GUI using the C4MLIT1, ISOSPI1, and BMS63EN boards. At this point in time, I am only interested in the logging functionality and just want to use the demo as it comes.I have the hardware set up in centralized c...

Luke_A by Associate II
  • 2336 Views
  • 2 replies
  • 2 kudos

Resolved! AEK-MOT-TK200G1 SPC5-UDESTK - No JTAG client found !

Hello,I have been trying to connect to the AEK-MOT-TK200G1 using a SPC5-UDESTK.I tried UDE starter kit 5.02.04, and UDE starter kit 2021.05. I'm getting the following error: (Message from component 'PpcJtagTargIntf' :Can't connect target !)I have che...

pivic_0-1739098668282.png pivic_1-1739098730855.png pivic_2-1739098743940.png 20250209_110028.jpg
pivic by Associate II
  • 2058 Views
  • 3 replies
  • 0 kudos

Resolved! AEK-MCU-C4MLIT1 Debugging via AEKSMCU-SPC5LNK

Hello, I am trying to debug an example code on a recently bought AEK-MCU-C4MLIT1 Evaluation Board via AEKSMCU-SPC5LNK using OpenOCD. I am fairly new to Embedded Systems and Eclipse Environment so I have just been following instructions.  And things d...

Vipuls by Associate III
  • 3390 Views
  • 2 replies
  • 0 kudos

Resolved! Autodevkit Studio BMS Library Functions

Hey Community!I am trying to build a BMS for a 333V Battery using AEK-MCU-C4MLIT1 as the Master MCU, AEK-COM-ISOSPI1 as the translator and multiple AEK-POW-BMS63EN boards in a daisy chain.Although there are various examples provided in the SPC5Studio...

Vipuls by Associate III
  • 1124 Views
  • 1 replies
  • 0 kudos

Resolved! Adding breakpoint and debugging using UDE STK 2021

Hello everyone,I have been flashing the code written in AutDevKit Studio 2.4.0 using UDE STK 2021 for the AEK-AUD-C1D9031, which uses the SPC582B60E1 MCU. I want to start debugging the code line by line using breakpoints.Currently, I have the option ...