AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Doutb regarding Daisy chaining BMSCCTX with BMSCCTX

Hi team,I have seen example of C4MINI1 daisy chaining BMSCCTX with BMSCC which is working fine.I have 2 BMSCCTX, so i was wondering that i can connect 2 BMSCCTX for daisy chaining with C4MINI1.But i have noticed that in the datasheet of CCTX, the dai...

Amal_V by Associate III
  • 481 Views
  • 1 replies
  • 1 kudos

Resolved! Spi not working in AEK-POW-BMSCCTX

Hi team,I am trying to run BMSCCTX using Pi as MCU. 1. I read the L9963 E and L9963 T datasheets. i found that any 8 bit message wakes up the BMS , i tried sending sample messages like 8 bit zeros and was able to turn on d2 led of bms.if the wake up ...

Amal_V by Associate III
  • 616 Views
  • 2 replies
  • 0 kudos

Resolved! SPC564L60L programer

Hi. I'm looking for a programmer for SPC564L60L5. The best would seem SPC5-UDESTK but it is not available for sale. Or maybe StellarLINK It will be ok for full programming and debugging support for this chip. Or maybe some other suggestions of a prog...