AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Battery management system

Hi, I am looking to use AEK-POW-BMSWTX battery management system for EV related battery management experiments. Please let me know if I can use AEK-POW-BMSWTX with STM32 microcontroller boards. Also please let me know if any other boards are required...

Resolved! FAD903D volume control

hi community  i am using  "AEK-AUD-C1D9031"  board. in this board i had flashed  .WAV files and i had played. the wave files are played using an example code given in the autodevkit. i used an API playsound() this one will give good sound when i had ...

image.png

Resolved! AEK-MCU-LNKU Debugger por SPC56

Hello, I have been trying to make the AEK-MCU-LNK work with my SPC56 discovery board with OPENOCD (I reached a dead end trying to make the .cgf files). So I have two questions:1.- I understand that the AEK-MCU-LNKU works with this SPC56 family using ...

Agustin by Associate II
  • 1410 Views
  • 3 replies
  • 2 kudos

Resolved! SPC58 EE84E7 SVD file problems accessing peripherals

Dear community,I am currently working with the SPC58 E-Line processor placed in the mother daughter evaluation board.I am using the AEK-MCU-SPC5LNK with OpenOCD. The reference manual for the E-Line is similar o the G-Line. I have only found the SVD f...

TKorn by Associate III
  • 400 Views
  • 4 replies
  • 1 kudos

Resolved! Issue with SPI between BMSCCTX and C4MINI

Hello team,I am using the GUI demo (single) for BMSCCTX and C4MINI with 4 LFP Batteries. I have followed the steps described by @ritehracingteam in this thread.After I run the program from the AutoDevKit Studio, my D9 and D2 LED are lit up and D8(Blu...

Zen432 by Associate II
  • 771 Views
  • 4 replies
  • 1 kudos

Resolved! Doutb regarding Daisy chaining BMSCCTX with BMSCCTX

Hi team,I have seen example of C4MINI1 daisy chaining BMSCCTX with BMSCC which is working fine.I have 2 BMSCCTX, so i was wondering that i can connect 2 BMSCCTX for daisy chaining with C4MINI1.But i have noticed that in the datasheet of CCTX, the dai...

Amal_V by Associate III
  • 450 Views
  • 1 replies
  • 1 kudos